User tip: a better bootargs_mmc env variable in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

User tip: a better bootargs_mmc env variable in u-boot

1,093件の閲覧回数
JohnReed
Contributor I

Refer to section 8.2 of this document:       i.MX53_START_Linux_BSP_UserGuide.pdf

 

In that section there is a recommended setting for the variable:  bootargs_mmc.

Adding:    ip=dhcp

will get u-boot to initialize eth0 and get an IP address.

 

If I did not have that parameter set, I found that I had to manually perform an ifconfig in order to bring up eth0 and assign an ip address (all after the system had come up and I logged in)

The other thing to note is that I'm running on a pretty minimal build.  Not quite the bare minimum, but almost.      See my earlier post:

http://imxcommunity.org/group/imx53quickstartboard/forum/topics/user-experience-with-1109-binaries-w...

 

Here's my setting so you can use copy/paste:

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 ip=dhcp rootwait rw video=mxcdi1fb:GBR24,VGA-XGA di1_primary vga'

 

JR

タグ(1)
0 件の賞賛
返信
0 返答(返信)