To Get a clean kernel source code from kernel.org with a tag of 2.6.35.3:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To Get a clean kernel source code from kernel.org with a tag of 2.6.35.3:

3,720 Views
admin
Specialist II

Hi,

I am facing the below problem in getting the kernel source code from
kernel.org with the tag of 2.6.35.3

ubuntu@ubuntu-laptop:~/IMX_

Android$ git clone
git://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-2.6.35.y.git
kernel_imx
Initialized empty Git repository in /home/ubuntu/IMX_Android/
kernel_imx/.git/
fatal: The remote end hung up unexpectedly

Could ne body pls kindly do the needful in resolving the above issue
so that i can get the kernel source code downloaded without ne issues

ne help would be greatly appreciated

Advanced thnks,
Srinivasan
mail id:[email protected]
Tags (1)
0 Kudos
Reply
2 Replies

3,233 Views
daiane_angolini
NXP Employee
NXP Employee

Yes, it was updated before kernel.org become offline.

 

Please use the procedure I posted on the other post you created:

http://imxcommunity.org/forum/topics/problem-in-getting-android-source-code-from-google-repo-as-per-...

0 Kudos
Reply

3,233 Views
daiane_angolini
NXP Employee
NXP Employee

It's working for me:

 

git clone https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
Initialized empty Git repository in /home/angolini/teste/linux/.git/
remote: Counting objects: 743584  

 

 

http://git.kernel.org/?p=linux/kernel/git/torvalds/linux.git;a=summary

0 Kudos
Reply