Use the eSDHC ,CMD0 issue error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use the eSDHC ,CMD0 issue error

1,366件の閲覧回数
sunsun
Contributor I

Hello!

When I use the eSDHC module,I try to issue the CMD0 commend to SD Card,one error was occur。

I am sure ,the I/O configuration is right, and the waveform,as follows:

Can see CMD0 send abort,and as the same time ,the bit 18 (CEBE)and the bit 17(CCE)of Interrupt Status Register (IRQSTAT) is ‘1’。

pastedImage_1.png

Can you give me some suggestion to save this problem?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,290件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sun

this may be hardware issue and one can try with baremetal sdk test

checking signals with oscilloscope

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/usdhc at master · RT-Thread/rt-thread · GitHub 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信