MIMXRT1064-EVK SPI DNP ports

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1064-EVK SPI DNP ports

1,607件の閲覧回数
greenad
Contributor I

I am using the MIMXRT1064-EVK for a project that involves using the SPI on the board. When looking through the schematics there is a DNP on the ports for the SPI clock, MOSI, MISO, and CS. Is there anyway to get around this or do I need to use a different board. Also does anybody have SPI user notes?

ラベル(1)
0 件の賞賛
返信
1 返信

1,523件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The R278, R279, R280, R281 are not mounted on the MIMXRT1064-EVKboard actually, to use the LPSPI interface, you should weld 0Ω resistor to R278, R279, R280, R281.
Hope this is clear.WeChat Image_20191105111749.jpg

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

 

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信