Use of ZMK instead of OTPMK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use of ZMK instead of OTPMK

ソリューションへジャンプ
1,033件の閲覧回数
gg_NXP_user
Contributor I

Hello,

I'm currently working on the i.Mx6.

I'm looking to modify the "master key".

It seems that the OTPMK key has already been fused on my board. By reading bit 0 of the SNVS_HP register, the OTPMK_ZERO bit is at 0.

However, the SSM_ST bit content is equal to 1011 (0xb), which means that my device is in Non-secure mode.

In this specific case, I can no longer modify the OTPMK key, is this correct?

Can I use the ZMK key instead of the OTPMK ?

What is the correct procedure to do that ?

Do I have to put the device in secure mode for the ZMK key to be taken into account?

Best Regards

0 件の賞賛
返信
1 解決策
996件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

I can no longer modify the OTPMK key, is this correct?

-> Correct, burned by Factory prior to shipping the device.

What is the correct procedure to do that?

-> Please refer to section 6.9.3. (ZMK programming guidelines)

 

Best regards

Harvey

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
997件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

I can no longer modify the OTPMK key, is this correct?

-> Correct, burned by Factory prior to shipping the device.

What is the correct procedure to do that?

-> Please refer to section 6.9.3. (ZMK programming guidelines)

 

Best regards

Harvey

 

0 件の賞賛
返信