Use of OEMDeviceTable in EC7 to configure uncached memory region

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use of OEMDeviceTable in EC7 to configure uncached memory region

2,174 Views
bdp42
Contributor IV

Hi,

I'm attempting to configure an area of memory that is uncached to address an issue I am having using the MS NOR strataflash driver. This is an Embedded Compact 7-based platform using an ARM processor. I've posted a related entry on this issue where I used a different approach to this problem. There I am using the MmMapIoSpace API to map this uncached region but am getting an alignment problem when using the NOR driver.

https://community.freescale.com/thread/307341

A different approach is to use the OEMDeviceTable to hard configure an uncached region for the NOR device. I've followed the instructions in the MSDN documentation. It looks straightforward but the system hangs somewhere in OS startup with no indication of what is wrong. The bootloader jumps to the image and then simply hangs.  Here's the relevant piece of the oemaddrtab_cfg.inc file

ALIGN
;------------------------------------------------------------------------------
;
; TABLE FORMAT
;       uncached address, physical address, size, attributes
;------------------------------------------------------------------------------
g_oalDeviceTable
    DCD 0x9D000000, CSP_BASE_MEM_PA_CS0/256, 1, 0      ; NOR Flash (uncached)
    DCD 0x00000000, 0x00000000, 0 , 0                   ; Terminate table

;------------------------------------------------------------------------------
;
; TABLE FORMAT
;       cached address, physical address, size
;------------------------------------------------------------------------------

g_oalAddressTable

    DCD CE_NEW_MAPPING_TABLE, g_oalDeviceTable, 0
    DCD 0x80000000, CSP_BASE_MEM_PA_CSD0, STATIC_MAPPING_RAM_SIZE           ; RAM image mapping
    DCD 0x9F100000, CSP_BASE_REG_PA_IPU_CM_1MB, 1       ; IPUv3 regs, CM,IDMAC,DP,DI0,DI1,DC,DMFC
    DCD 0x9F200000, CSP_BASE_REG_PA_IPU_CPMEM_1MB, 1    ; IPUv3 regs, CPMEM,SRM, DC template
    DCD 0x9F300000, CSP_BASE_REG_PA_SATA, 1             ; SATA regs
    DCD 0x9F400000, CSP_BASE_REG_PA_SATA_P0, 1          ; SATA P0 regs
    DCD 0x9F500000, CSP_BASE_MEM_PA_NFC_1MB, 5          ; NFC internal buffer
    DCD 0x9FA00000, CSP_BASE_MEM_PA_IRAM_1MB, 1         ; Internal RAM
    DCD 0x9FB00000, CSP_BASE_REG_PA_TZIC_1MB, 1         ; TZIC regs
    DCD 0x9FC00000, CSP_BASE_MEM_PA_ROM, 1              ; Internal ROM
    DCD 0x9FD00000, CSP_BASE_MEM_PA_AIPS1, 1            ; AIPS1 SPBA peripheral regs
    DCD 0x9FE00000, CSP_BASE_REG_PA_AIPS1, 1            ; AIPS1 peripheral regs
    DCD 0x9FF00000, CSP_BASE_REG_PA_AIPS2, 1            ; AIPS2 peripheral regs
    DCD 0x00000000, 0x00000000, 0                       ; Terminate table

;------------------------------------------------------------------------------

Is there anything obviously wrong here? Has anyone successfully used the OEMDeviceTable and are there any known issues? There seems little information about it on the forums.

Perhaps there is a different approach to address the problem?

Thanks,

Bruno



Labels (1)
0 Kudos
Reply
4 Replies

1,674 Views
YixingKong
Senior Contributor IV

Bruno

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

1,674 Views
bdp42
Contributor IV

This is going back a long time. We have moved on from this approach and this issue is not relevant any more.

Bruno

0 Kudos
Reply

1,674 Views
admin
Specialist II

Deactivated user,

Adeneo support - can you please help with this issue found on a WEC7 platform.  Thanks.

0 Kudos
Reply

1,674 Views
YixingKong
Senior Contributor IV

Deactivated user, so you have time to look into the customer's question?

Thanks,

Yixing

0 Kudos
Reply