Hi All,
We are working product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.
Is there any limitation that we can't use kmssink with eLCDIF?
Is there any way I can mitigate this limitation? Is it possible to use kmssink with eLCDIF?
Thanks,
Jemish
已解决! 转到解答。
Hi,
Please try to use videotestsrc first:
gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=falseIs this working? If so, then it is because your video resolution doesn't match the display. As said, it cannot scale, therefore resolutions have to match or you need to scale it via another plugin.
Regards,
Gary
Hi Joanxie
I have already written in my question that we are using "glimagesink" for LCD. But with that we observed some horizontal flickering on LCD screen. Attaching video for your reference.
But we drive LCD via DCSS using kmsink we don't see these artifacts.
If there is any limitation that we can't use kmssink with eLCDIF then it's fine but I want to know the reason behind it. Why can't we use kmssink with eLCDIF?
Thanks,
Jemish
Hi,
There's nothing preventing you from using kmssink SW-wise on eLCDIF.
We've been supporting kmssink on our boards and it works fine. Couple of things to note:
- drm driver name is mxsfb-drm, you might need to specify it to the kmssink as parameter
- this kms driver doesn't support scaling, unlike DCSS, so you also might need to specify 'can-scale=false'
Regards,
Gary
Hi Gary,
Thanks for you input. I tried your suggestion on same day you provided. And replied back on that day. Something went wrong on this thread. And somehow I don't see my reply so today I am posting again.
Unfortunately your suggestion didn't work for me and I am still getting following error.
# gst-launch-1.0 filesrc location=animation-1.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! kmssink driver-name="mxsfb-drm" can-scale=false
Setting pipeline to PAUSED ...
====== VPUDEC: 4.4.5 build on Jul 9 2020 09:54:35. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jul 9 2020 09:54:03)
vpulib: 1.1.1
firmware: 1.1.1.65535
Pipeline is PREROLLING ...
====== AIUR: 4.4.5 build on Jul 9 2020 09:54:29. ======
Core: MPEG4PARSER_06.16.01 build on Dec 11 2018 03:04:17
file: /usr/lib/lib_mp4_parser_arm_elinux.so
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:03.500000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)800, framerate=(fraction)24/1, codec_data=(buffer)01640020ffe1001967640020acd9405
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:03.568000000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)2298, stream-format=(string)raw, codec_data=(buffer)119056e500
------------------------
ERROR: from element /GstPipeline:pipeline0/GstQueue:queue0: Internal data stream error.
Additional debug info:
gstqueue.c(1566): gst_queue_loop (): /GstPipeline:pipeline0/GstQueue:queue0:
streaming stopped, reason not-negotiated (-4)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
Do you have any further suggestions?
Thanks,
Jemish
Hi,
Please try to use videotestsrc first:
gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=falseIs this working? If so, then it is because your video resolution doesn't match the display. As said, it cannot scale, therefore resolutions have to match or you need to scale it via another plugin.
Regards,
Gary
Hi Gary,
Thanks for you input. Test pattern works for me with minor change in command.
gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=false force-modesetting=true.
Yes I am aware the eLCDIF doesn't support scaling so I kept MP4 video of same resolution as LCD (1280x800). Still I am getting same error .
ERROR: from element /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.
To understand error in detail I enabled log level and I am getting following message:
aiurdemux aiurdemux.c:3421:aiurdemux_push_pad_buffer: Pad audio push error type -1
basetransform gstbasetransform.c:1355:gst_base_transform_setcaps:<videoconvert0> transform could not transform video/x-raw, format=(string)NV12, width
=(int)1280, height=(int)800, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flippe
d/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, chroma-site=(string)mpeg2, colorimetry=(string)bt709, framerate=(fraction)24000/1001 in anything we support
aiurdemux aiurdemux.c:3421:aiurdemux_push_pad_buffer: Pad video push error type -4
As per my understanding eLCDIF doesn't support color conversion also. That's the reason I am getting the above error. So I have to convert video in way that eLCDIF supports. Correct me if I am wrong.
Do you have any further suggestion?
Thanks,
Jemish
Hi Gary,
Thanks for you input. I tried command as you suggested but it still failed to start video and gives an error.
I am pasting log for command.Do you have further suggestion?
gst-launch-1.0 filesrc location=animation-1.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! kmssink driver-name="mxsfb-drm" can-scale=false
Setting pipeline to PAUSED ...
====== VPUDEC: 4.4.5 build on Jul 9 2020 09:54:35. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jul 9 2020 09:54:03)
vpulib: 1.1.1
firmware: 1.1.1.65535
Pipeline is PREROLLING ...
====== AIUR: 4.4.5 build on Jul 9 2020 09:54:29. ======
Core: MPEG4PARSER_06.16.01 build on Dec 11 2018 03:04:17
file: /usr/lib/lib_mp4_parser_arm_elinux.so
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:03.500000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)800, framerate=(fraction)24/1, codec_data=(buffer)01640020ffe1001967640020acd9405
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:03.568000000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)2298, stream-format=(string)raw, codec_data=(buffer)119056e500
------------------------
ERROR: from element /GstPipeline:pipeline0/GstQueue:queue0: Internal data stream error.
Additional debug info:
gstqueue.c(1566): gst_queue_loop (): /GstPipeline:pipeline0/GstQueue:queue0:
streaming stopped, reason not-negotiated (-4)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...
Thanks,
Jemish