Use kmssink with elcdif on IMX8MQ processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use kmssink with elcdif on IMX8MQ processor

跳至解决方案
8,511 次查看
jemish_1990
Contributor V

Hi All,

We are working product based on IMX8MQ (MIMX8MQ6DVAJZAA) processor.

  • In our board we are using two displays.
  • We are using LCD via eLCDIF + MIPI and HDMI via DCSS.
  • In our case currently we are rendering video on LCD using glimagesink and HDMI using kmssink.
  • We display preview captured via camera on LCD. In that usecase we observed some horizontal flickering on LCD screen.
  • To debug this issue we use LCD using DCSS (which is driven by kmssink). And we don't see issue.
  • In imx8mq release note I see that kmssink is used only with DCSS and glimagesink with eLCDIF.

Is there any limitation that we can't use kmssink with eLCDIF?

Is there any way I can mitigate this limitation? Is it possible to use kmssink with eLCDIF?

Thanks,

Jemish

 

0 项奖励
回复
1 解答
8,438 次查看
gary_bisson
Senior Contributor III

Hi,

Please try to use videotestsrc first:

gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=false

Is this working? If so, then it is because your video resolution doesn't match the display. As said, it cannot scale, therefore resolutions have to match or you need to scale it via another plugin.

Regards,

Gary

在原帖中查看解决方案

0 项奖励
回复
12 回复数
8,492 次查看
joanxie
NXP TechSupport
NXP TechSupport

why don't you use glimagesink or waylandsink to replace kmssink? I suggest that you can use glimagesink

0 项奖励
回复
8,475 次查看
jemish_1990
Contributor V

Hi Joanxie

I have already written in my question that we are using "glimagesink" for LCD. But with that we observed some horizontal flickering on LCD screen. Attaching video for your reference.

But we drive LCD via DCSS using kmsink we don't see these artifacts.

If there is any limitation that we can't use kmssink with eLCDIF then it's fine  but I want to know the reason behind it. Why can't we use kmssink with eLCDIF?

Thanks,

Jemish

 

 

0 项奖励
回复
8,465 次查看
jemish_1990
Contributor V

Hi NXP team,

Any update on this?

Thanks,

Jemish

0 项奖励
回复
8,456 次查看
gary_bisson
Senior Contributor III

Hi,

There's nothing preventing you from using kmssink SW-wise on eLCDIF.

We've been supporting kmssink on our boards and it works fine. Couple of things to note:

- drm driver name is mxsfb-drm, you might need to specify it to the kmssink as parameter

- this kms driver doesn't support scaling, unlike DCSS, so you also might need to specify 'can-scale=false'

Regards,

Gary

0 项奖励
回复
8,435 次查看
jemish_1990
Contributor V

Hi Gary,

Thanks for you input. I tried your suggestion on same day you provided. And replied back on that day. Something went wrong on this thread. And somehow I don't see my reply so today I am posting again.

Unfortunately your suggestion didn't work for me and I am still getting following error. 

# gst-launch-1.0 filesrc location=animation-1.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! kmssink driver-name="mxsfb-drm" can-scale=false
Setting pipeline to PAUSED ...
====== VPUDEC: 4.4.5 build on Jul 9 2020 09:54:35. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jul 9 2020 09:54:03)
vpulib: 1.1.1
firmware: 1.1.1.65535
Pipeline is PREROLLING ...

====== AIUR: 4.4.5 build on Jul 9 2020 09:54:29. ======
Core: MPEG4PARSER_06.16.01 build on Dec 11 2018 03:04:17
file: /usr/lib/lib_mp4_parser_arm_elinux.so
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:03.500000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)800, framerate=(fraction)24/1, codec_data=(buffer)01640020ffe1001967640020acd9405
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:03.568000000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)2298, stream-format=(string)raw, codec_data=(buffer)119056e500
------------------------
ERROR: from element /GstPipeline:pipeline0/GstQueue:queue0: Internal data stream error.
Additional debug info:
gstqueue.c(1566): gst_queue_loop (): /GstPipeline:pipeline0/GstQueue:queue0:
streaming stopped, reason not-negotiated (-4)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...

Do you have any further suggestions?

Thanks,

Jemish

0 项奖励
回复
8,439 次查看
gary_bisson
Senior Contributor III

Hi,

Please try to use videotestsrc first:

gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=false

Is this working? If so, then it is because your video resolution doesn't match the display. As said, it cannot scale, therefore resolutions have to match or you need to scale it via another plugin.

Regards,

Gary

0 项奖励
回复
8,419 次查看
jemish_1990
Contributor V

Hi Gary,

Thanks for you input. Test pattern works for me with minor change in command.

gst-launch-1.0 videotestsrc ! kmssink driver-name="mxsfb-drm" can-scale=false force-modesetting=true.

Yes I am aware the eLCDIF doesn't support scaling so I kept MP4 video of same resolution as LCD (1280x800). Still I am getting same error .

ERROR: from element /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.

To understand error in detail I enabled log level and I am getting following message:

aiurdemux aiurdemux.c:3421:aiurdemux_push_pad_buffer: Pad audio push error type -1

basetransform gstbasetransform.c:1355:gst_base_transform_setcaps:<videoconvert0> transform could not transform video/x-raw, format=(string)NV12, width
=(int)1280, height=(int)800, interlace-mode=(string)progressive, multiview-mode=(string)mono, multiview-flags=(GstVideoMultiviewFlagsSet)0:ffffffff:/right-view-first/left-flipped/left-flopped/right-flippe
d/right-flopped/half-aspect/mixed-mono, pixel-aspect-ratio=(fraction)1/1, chroma-site=(string)mpeg2, colorimetry=(string)bt709, framerate=(fraction)24000/1001 in anything we support

aiurdemux aiurdemux.c:3421:aiurdemux_push_pad_buffer: Pad video push error type -4

As per my understanding eLCDIF doesn't support color conversion also. That's the reason I am getting the above error. So I have to convert video in way that eLCDIF supports. Correct me if I am wrong.

Do you have any further suggestion?

Thanks,

Jemish

 

 

0 项奖励
回复
8,411 次查看
gary_bisson
Senior Contributor III

Hi,

Yes you might have to do a colorspace conversion, try adding a videoconvert plugin before the kmssink one.

Regards,

Gary

0 项奖励
回复
8,394 次查看
jemish_1990
Contributor V

Hi Gary,

Sorry for late reply!

Thanks a lot for your valuable inputs. We have concluded this task.

We can close this thread now.

Thanks,

Jemish

0 项奖励
回复
8,389 次查看
gary_bisson
Senior Contributor III

Hi,

Glad to hear it works! Please make sure to mark the answer that resolved the issue as best answer.

Thanks,

Gary

0 项奖励
回复
8,415 次查看
joanxie
NXP TechSupport
NXP TechSupport

what bsp version do you use? try to use the latest 5.4.24 version, I tested kmssink successfully just now

0 项奖励
回复
8,418 次查看
jemish_1990
Contributor V

Hi Gary,

Thanks for you input. I tried command as you suggested but it still failed to start video and gives an error.

I am pasting log for command.Do you have further suggestion?

gst-launch-1.0 filesrc location=animation-1.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! kmssink driver-name="mxsfb-drm" can-scale=false
Setting pipeline to PAUSED ...
====== VPUDEC: 4.4.5 build on Jul 9 2020 09:54:35. ======
wrapper: 3.0.0 (VPUWRAPPER_ARM64_LINUX Build on Jul 9 2020 09:54:03)
vpulib: 1.1.1
firmware: 1.1.1.65535
Pipeline is PREROLLING ...

====== AIUR: 4.4.5 build on Jul 9 2020 09:54:29. ======
Core: MPEG4PARSER_06.16.01 build on Dec 11 2018 03:04:17
file: /usr/lib/lib_mp4_parser_arm_elinux.so
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:03.500000000
Language: eng
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1280, height=(int)800, framerate=(fraction)24/1, codec_data=(buffer)01640020ffe1001967640020acd9405
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:03.568000000
Language: eng
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)48000, bitrate=(int)2298, stream-format=(string)raw, codec_data=(buffer)119056e500
------------------------
ERROR: from element /GstPipeline:pipeline0/GstQueue:queue0: Internal data stream error.
Additional debug info:
gstqueue.c(1566): gst_queue_loop (): /GstPipeline:pipeline0/GstQueue:queue0:
streaming stopped, reason not-negotiated (-4)
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
Freeing pipeline ...

 

Thanks,

Jemish

0 项奖励
回复