Use hardware acceleration with i.MX 8MQ using GStreamer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use hardware acceleration with i.MX 8MQ using GStreamer

382 Views
Justin17000
Contributor I

I'm working on a i.MX 8MQ with Debian and a kernel aarch64 Linux 5.15.60.

I'm trying to decode a mp4 video using the pipeline I found in the i.MX 8 GStreamer user guide :

gst-launch-1.0 filesrc location=<filename.mp4> ! qtdemux name=d d.video_0 ! queue ! h264parse ! vpudec ! queue ! waylandsink 

I get the following error : 

ERROR: from element /GstPipeline:pipeline0/GstVpuDec:vpudec0: Could not initialize supporting library
Additional debug info:
gstvideodecoder.c(2352) : gst_video_decoder_change_state (): /GstPipeline:pipeline0/GstVpuDec:vpudec0:
Failed to start decoder

I've tried to get the v4l2h264dec by downloading gstreamer1.0-plugins-bad via apt (didn't get the plugin) and by cloning the Github repositery (didn't get the plugin).


 

0 Kudos
Reply
1 Reply

343 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The oficial BSP work with yocto where you installed the image-full and you get gstreamer, if you are on debian or other non supported by nxp you need to download and install yourself.

Regards

0 Kudos
Reply