Use PCIe X1 for M.2 NVMe SSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Use PCIe X1 for M.2 NVMe SSD

7,466件の閲覧回数
x10
Contributor V

Hi, All

Is it possible to use the mini PCIe in iMX7D SABRD to connect an M.2 nvme ssd, with an adapter of course? The M.2 nvme module can be either PCIe X2 key B+M, or PCIe X4 key M. As my understanding, PCIe X1 should be work with these modules with lower speed which is fine enough in embedded applications.

Thanks for help in advance.

Cheng Shi

ラベル(2)
0 件の賞賛
返信
6 返答(返信)

6,355件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cheng 

yes, since i.MX7D has PCI Express port (PCIe) v. 2.1 with one lane

seems there should be no problems for using that device.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,355件の閲覧回数
kevinchan
Contributor I

I have tested the SSD M.2 nvme ssd, with an  adapter mini-PCIE to M2 on iMX7D SABRD but doesn't work.

Any idea?

0 件の賞賛
返信

6,355件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

is it detected, if not one can look on

I.MX7 PCIe phy link never came up 

Best regards
igor

0 件の賞賛
返信

6,355件の閲覧回数
kevinchan
Contributor I

I tried different M.2 SSD on Sabre board with mini-PCIE to M.2 adaptor.

- Kingston A1000 - can be detected and work normal.

- Western Digital SN520 - can't be detected

- Foresee P900F128G - can't be detected.

Please advise what's wrong!

0 件の賞賛
返信

6,355件の閲覧回数
x10
Contributor V

KINGSHARE KEN800128SSD.

KINGSpec M2 128GB NVME

MZ - FLW1280

Above three typies of NVMe modules are worked with my customer iMX7D board.

0 件の賞賛
返信

6,355件の閲覧回数
ao2
Contributor I

Which mini-PCIE to M.2 adapter have you used? Could you please send me a product link of this adapter?

Thank you very much.

Best regards

Andreas

0 件の賞賛
返信