Use PCIe X1 for M.2 NVMe SSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use PCIe X1 for M.2 NVMe SSD

4,096 Views
x10
Contributor V

Hi, All

Is it possible to use the mini PCIe in iMX7D SABRD to connect an M.2 nvme ssd, with an adapter of course? The M.2 nvme module can be either PCIe X2 key B+M, or PCIe X4 key M. As my understanding, PCIe X1 should be work with these modules with lower speed which is fine enough in embedded applications.

Thanks for help in advance.

Cheng Shi

Labels (2)
0 Kudos
6 Replies

2,985 Views
igorpadykov
NXP Employee
NXP Employee

Hi Cheng 

yes, since i.MX7D has PCI Express port (PCIe) v. 2.1 with one lane

seems there should be no problems for using that device.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,985 Views
kevinchan
Contributor I

I have tested the SSD M.2 nvme ssd, with an  adapter mini-PCIE to M2 on iMX7D SABRD but doesn't work.

Any idea?

0 Kudos

2,985 Views
igorpadykov
NXP Employee
NXP Employee

is it detected, if not one can look on

I.MX7 PCIe phy link never came up 

Best regards
igor

0 Kudos

2,985 Views
kevinchan
Contributor I

I tried different M.2 SSD on Sabre board with mini-PCIE to M.2 adaptor.

- Kingston A1000 - can be detected and work normal.

- Western Digital SN520 - can't be detected

- Foresee P900F128G - can't be detected.

Please advise what's wrong!

0 Kudos

2,985 Views
x10
Contributor V

KINGSHARE KEN800128SSD.

KINGSpec M2 128GB NVME

MZ - FLW1280

Above three typies of NVMe modules are worked with my customer iMX7D board.

0 Kudos

2,985 Views
ao2
Contributor I

Which mini-PCIE to M.2 adapter have you used? Could you please send me a product link of this adapter?

Thank you very much.

Best regards

Andreas

0 Kudos