Use ADDR and READ command when ddr_mode_enable parameter is 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use ADDR and READ command when ddr_mode_enable parameter is 1

2,034 Views
ko-hey
Senior Contributor II

Hi all

 

I have a question about QSPI nor flash config file such as qspi-nor-xxx-config and this thread is related following thread.

https://community.nxp.com/thread/490051

 

My customer use N25Q032A of micron and the config file setting is as follow.

They have already launched with the flash and the settings.

 

Setting a "ddr_mode_enable = 1"

Use ADDR and READ

The command sequence set for lut is as follows

 

      CMD - Read Zero Latency(03h)

      ADDR

      READ

      JMP_ON_CS

 

With the above settings, the program can be loaded from the NOR flash memory and executed.

Their biggest concern is whether or not the loading of the program in the NOR flash may fail due to the above setting.

 

 

Is there a possibility that program loading will fail with the above settings ?

 

 

Ko-hey

 

Labels (4)
0 Kudos
Reply
4 Replies

1,819 Views
art
NXP Employee
NXP Employee

Unfortunately, your customer's task is not exactly clear for me. Does the customer want to load a code from QSPI NOR Flash to RAM and then execute it from there? And, their main concern is that the code may become corrupted when copying it from QSPI NOR Flash to RAM, am I correct? Please specify.

Best Regards,
Artur

0 Kudos
Reply

1,819 Views
ko-hey
Senior Contributor II

Hi Artur Petukhov

We would like to know if loading may fail at the time of deployment from QSPI to RAM during boot.

Ko-hey

0 Kudos
Reply

1,819 Views
ko-hey
Senior Contributor II

Hi Artur Petukhov

Could you follow and answer this thread ?

Ko-hey

0 Kudos
Reply

1,819 Views
ko-hey
Senior Contributor II

Hi art

Could you follow this thread ?

Ko-hey

0 Kudos
Reply