Unused pin treatment about VDD1P5 of i.MX28

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unused pin treatment about VDD1P5 of i.MX28

跳至解决方案
1,051 次查看
torus1000
Contributor V

Hi

Please tell us about VDD1P5 of i.MX28.

In my design, there is no LV-DDR2 memory and
it is just connected to the capacitors(0.01uF ~ 22uF).

In this case, is it OK to eliminate these capacitors ?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
886 次查看
MarekVasut
Senior Contributor I

You can disable the 1V5 linreg via HW_POWER_VDDMEMCTRL : ENABLE_LINREG register/bit, then you should be fine not connecting anything to the pad.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
886 次查看
YixingKong
Senior Contributor IV

Torus1000

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复
886 次查看
YixingKong
Senior Contributor IV

Torus1000


Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 项奖励
回复
887 次查看
MarekVasut
Senior Contributor I

You can disable the 1V5 linreg via HW_POWER_VDDMEMCTRL : ENABLE_LINREG register/bit, then you should be fine not connecting anything to the pad.

0 项奖励
回复