Unused pin treatment about VDD1P5 of i.MX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused pin treatment about VDD1P5 of i.MX28

Jump to solution
1,005 Views
torus1000
Contributor V

Hi

Please tell us about VDD1P5 of i.MX28.

In my design, there is no LV-DDR2 memory and
it is just connected to the capacitors(0.01uF ~ 22uF).

In this case, is it OK to eliminate these capacitors ?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
840 Views
MarekVasut
Senior Contributor I

You can disable the 1V5 linreg via HW_POWER_VDDMEMCTRL : ENABLE_LINREG register/bit, then you should be fine not connecting anything to the pad.

View solution in original post

0 Kudos
Reply
3 Replies
840 Views
YixingKong
Senior Contributor IV

Torus1000

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply
840 Views
YixingKong
Senior Contributor IV

Torus1000


Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel

free to contact Freescale.

Thanks,
Yixing

0 Kudos
Reply
841 Views
MarekVasut
Senior Contributor I

You can disable the 1V5 linreg via HW_POWER_VDDMEMCTRL : ENABLE_LINREG register/bit, then you should be fine not connecting anything to the pad.

0 Kudos
Reply