Unit_tests porting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,394件の閲覧回数
xu_ji1
Contributor V

Hi,

I want to porting the unit_tests module that in Yocto project to Android project.

Does it feasible? Please give guide.

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,269件の閲覧回数
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,269件の閲覧回数
art
NXP Employee
NXP Employee

There seems to be no way to directly port the unit_tests application from Linux to Android. A new Android application should be created from the scratch.

Best Regards,
Artur

0 件の賞賛
返信
3,270件の閲覧回数
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

0 件の賞賛
返信
3,269件の閲覧回数
art
NXP Employee
NXP Employee

Yes, it's OK.

0 件の賞賛
返信
3,269件の閲覧回数
xu_ji1
Contributor V

What is the scratch?

0 件の賞賛
返信
3,269件の閲覧回数
art
NXP Employee
NXP Employee

"From the scratch" is the idiomatic phrase that means "from the very beginning stage".

0 件の賞賛
返信