Unit_tests porting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unit_tests porting

跳至解决方案
2,457 次查看
xu_ji1
Contributor V

Hi,

I want to porting the unit_tests module that in Yocto project to Android project.

Does it feasible? Please give guide.

Thanks

0 项奖励
回复
1 解答
2,332 次查看
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,332 次查看
art
NXP Employee
NXP Employee

There seems to be no way to directly port the unit_tests application from Linux to Android. A new Android application should be created from the scratch.

Best Regards,
Artur

0 项奖励
回复
2,333 次查看
xu_ji1
Contributor V

What is the scratch?If I porting one module of Unit_tests like camera,is it ok?

Thanks

0 项奖励
回复
2,332 次查看
art
NXP Employee
NXP Employee

Yes, it's OK.

0 项奖励
回复
2,332 次查看
xu_ji1
Contributor V

What is the scratch?

0 项奖励
回复
2,332 次查看
art
NXP Employee
NXP Employee

"From the scratch" is the idiomatic phrase that means "from the very beginning stage".

0 项奖励
回复