imx6q 4.1.15 kernel framebuffer rotate left90 degree with multibuffer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q 4.1.15 kernel framebuffer rotate left90 degree with multibuffer

1,869 次查看
jiujinhong
Contributor IV

Hi,

I have applied patch in attach for imx6q 4.1.15 framebuffer rotate. it working fine. but later framebuffer set_par with 3 page flip buffer through below code in another driver, IPU SDC will update fail.  if FB0_FLIP_BUFFER_NUM use 1, it works fine.

[   13.333544] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A800000, current buf 1, buf0 ready 1, buf1 ready 1, buf2 ready 0
[   13.447193] mxc_sdc_fb fb@0: Error updating SDC buf 1 to address=0x1AB00000, current buf 1, buf0 ready 1, buf1 ready 0, buf2 ready 0
[   13.563912] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A500000, current buf 1, buf0 ready 1, buf1 ready 1, buf2 ready 0
[   13.771218] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1AB00000, current buf 0, buf0 ready 0, buf1 ready 1, buf2 ready 0
[   14.000068] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A800000, current buf 0, buf0 ready 0, buf1 ready 1, buf2 ready 0
[   14.119145] mxc_sdc_fb fb@0: Error updating SDC buf 1 to address=0x1AB00000, current buf 0, buf0 ready 1, buf1 ready 1, buf2 ready 0
[   14.335582] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A800000, current buf 1, buf0 ready 1, buf1 ready 1, buf2 ready 0
[   14.541331] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A500000, current buf 0, buf0 ready 0, buf1 ready 1, buf2 ready 0
[   14.639933] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A800000, current buf 1, buf0 ready 1, buf1 ready 1, buf2 ready 0
[   14.845036] mxc_sdc_fb fb@0: Error updating SDC buf 0 to address=0x1A500000, current buf 0, buf0 ready 0, buf1 ready 1, buf2 ready 0

#define FB0_FLIP_BUFFER_NUM  3

6   fbi_fb0 = registered_fb[0];                                                                                             
 15   if(fbi_fb0 == NULL){                                                                                                    
 14     return -1;                                                                                                            
 13   }                                                                                                                       
 12   memcpy(&var, &fbi_fb0->var, sizeof(var));                                                                               
 11   console_lock();                                                                                                         
 10   fbi_fb0->flags |= FBINFO_MISC_USEREVENT;                                                                                
  9   var.xres_virtual = ALIGN_PIXEL_16(var.xres);                                                                            
  8   var.yres_virtual = ALIGN_PIXEL_16(var.yres) * FB0_FLIP_BUFFER_NUM;                                                      
  7   fb_set_var(fbi_fb0, &var);                                                                                              
  6   fbi_fb0->flags &= ~FBINFO_MISC_USEREVENT;                                                                               
  5   console_unlock(); 

标签 (3)
0 项奖励
回复
3 回复数

1,552 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   Have You tried the following example(s) ?

"ipu-examples release notes - v0.1"

https://community.nxp.com/docs/DOC-94961

https://github.com/rogeriorps/ipu-examples


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,552 次查看
jiujinhong
Contributor IV

Hi,

No, just run with Android OS(Android N) directly.

0 项奖励
回复

1,552 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   perhaps it makes sense to apply to 

https://www.nxp.com/support/support/nxp-professional-services:PROFESSIONAL-SERVICE

Regards,

Yuri.

0 项奖励
回复