Unique Chip ID of RT1176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unique Chip ID of RT1176

1,193 Views
Stephan_
Contributor I

Hi,

according reference manual there is a unique chip ID stored in On-Chip OTP module. But I can't find any information how the read out this information.

Would be helpful if someone can give me hint how to read out this information.

Best Regards

Labels (1)
0 Kudos
Reply
1 Reply

1,183 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The below two registers contain the unique 64-bit chip ID.

jeremyzhou_0-1642125778811.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply