Unique Chip ID of RT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unique Chip ID of RT1176

1,237件の閲覧回数
Stephan_
Contributor I

Hi,

according reference manual there is a unique chip ID stored in On-Chip OTP module. But I can't find any information how the read out this information.

Would be helpful if someone can give me hint how to read out this information.

Best Regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,227件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The below two registers contain the unique 64-bit chip ID.

jeremyzhou_0-1642125778811.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信