Unfortunately the process com.android.phone has stopped pop-up window coming continously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unfortunately the process com.android.phone has stopped pop-up window coming continously

3,862件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi all,

After android booting in UI "unfortunately the process com.android.phone has stopped" pop-up coming continuously. how to fix it.

LOGCAT:

  root@sabresd_6dq:/ # logcat 

--------- beginning of /dev/log/main

W/AudioService( 1029): onLoadSoundEffects() called before boot complete

I/Process ( 1277): Sending signal. PID: 1277 SIG: 9

--------- beginning of /dev/log/system

I/ActivityManager( 1029): Process com.android.phone (pid 1277) has died.

I/ActivityManager( 1029): Start proc com.android.phone for restart com.android.phone: pid=1299 uid=1001 gids={41001, 3002, 3001, 3003, 1028, 1015}

D/AndroidRuntime( 1299): Shutting down VM

W/dalvikvm( 1299): threadid=1: thread exiting with uncaught exception (group=0x2c56cba8)

E/AndroidRuntime( 1299): FATAL EXCEPTION: main

E/AndroidRuntime( 1299): Process: com.android.phone, PID: 1299

E/AndroidRuntime( 1299): java.lang.RuntimeException: Unable to create application com.android.phone.PhoneApp: java.lang.NullPointerException: missing IConnectivityManager

E/AndroidRuntime( 1299): at android.app.ActivityThread.handleBindApplication(ActivityThread.java:4331)

E/AndroidRuntime( 1299): at android.app.ActivityThread.access$1500(ActivityThread.java:135)

E/AndroidRuntime( 1299): at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1256)

E/AndroidRuntime( 1299): at android.os.Handler.dispatchMessage(Handler.java:102)

E/AndroidRuntime( 1299): at android.os.Looper.loop(Looper.java:136)

E/AndroidRuntime( 1299): at android.app.ActivityThread.main(ActivityThread.java:5001)

E/AndroidRuntime( 1299): at java.lang.reflect.Method.invokeNative(Native Method)

E/AndroidRuntime( 1299): at java.lang.reflect.Method.invoke(Method.java:515)

E/AndroidRuntime( 1299): at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:785)

E/AndroidRuntime( 1299): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:601)

E/AndroidRuntime( 1299): at dalvik.system.NativeStart.main(Native Method)

E/AndroidRuntime( 1299): Caused by: java.lang.NullPointer

Regards,

Aravinth

0 件の賞賛
返信
2 返答(返信)

2,298件の閲覧回数
bestwaymk
Contributor I

you need to clear data and cache of SIM Toolkit

you can found other solutions here

0 件の賞賛
返信

2,298件の閲覧回数
art
NXP Employee
NXP Employee

The most likely cause of the issue is that the Phone application doesn't find the actual phone communication hardware present in the system. Just avoid to start the Phone application.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信