Unable to see video on FSL gnome - please help!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to see video on FSL gnome - please help!

2,247 Views
danix
Contributor III

Hi all,

I'm using fsl Gnome release on imx233. I build it with all gstreamer plugins and fsl multimedia codecs and libs.

 

totem plays the audio, but no video on screen. If I use gplay it plays both video and audio smoothly. But I want to use my device standalone, and hence need to launch it from the device using the tough screen.

 

Please, any hint would be appreciated.....

Tags (1)
0 Kudos
Reply
6 Replies

1,871 Views
daiane_angolini
NXP Employee
NXP Employee

Aren´t you using Ubuntu rootfs from FSL site? I supposed you was.

 

Yes, I suppose Totem is using default video sink, I only don´t know which video sink is the default one =P

 

For screen size, I mean the totem window dimension. Try to use totem maximized.

0 Kudos
Reply

1,871 Views
danix
Contributor III

Totem is using the default video sink, I guess

 

What do you mean by Ubuntu binary? .... (i'm using imx233 on a custom board btw.)

 

My screen resolution is 320x240, (3.5" TFT)

 

The fsl command line player shows almost the same log, but it plays smoothly rendering high quality video!

0 Kudos
Reply

1,871 Views
daiane_angolini
NXP Employee
NXP Employee

It is decoding movie too but this is not showing on screen. I think the issue is on videosink totem uses. Do you know which video sink totem uses?

 

Is there some new Ubuntu binary you can donwload?

 

Another thing I just remembered. How small is your totem screen? I know some codec (in fact, I don´t know if it´s for decoder or video sink) cannot handle very small windows screens (I thinks it´s because the resize ratio for IPU)

 

 

I don´t have anything else to add =(

0 Kudos
Reply

1,871 Views
danix
Contributor III

Hi Daiane,

I connected my device to a PC rs-232 terminal and got the following log when I launch totem using the GUI on device. I opened from there a 3min mp4 video (MPEG-4, AAC), which plays well with 'gplay' on another rootfs.

     < I can hear the audio clearly, but all I can see is a black window on the LCD.>

.

.

.

MFW_GST_V4LSINK_PLUGIN 1.8.0 build on May 31 2011 18:26:42.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs

** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/jamendo/jamendo.totem-plugin', Totem was not compiled with Python support

** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/jamendo/jamendo.totem-plugin

** (totem:925): WARNING **: Failed to create dbus proxy for org.gnome.SettingsDaemon: Could not get owner of name 'org.gnome.SettingsDaemon': no such name

** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/coherence_upnp/coherence_upnp.totem-plugin', Totem was not compiled with Python support

** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/coherence_upnp/coherence_upnp.totem-plugin

** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/opensubtitles/opensubtitles.totem-plugin', Totem was not compiled with Python support

** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/opensubtitles/opensubtitles.totem-plugin

** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/pythonconsole/pythonconsole.totem-plugin', Totem was not compiled with Python support

** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/pythonconsole/pythonconsole.totem-plugin

** (totem:925): WARNING **: Cannot load Python extension '/usr/lib/totem/plugins/youtube/youtube.totem-plugin', Totem was not compiled with Python support

** (totem:925): WARNING **: Failed to load plugin file: /usr/lib/totem/plugins/youtube/youtube.totem-plugin
MPEG4PARSER_06.01.08  build on Mar  3 2010 17:08:43.
MFW_GST_MP4_PARSER_PLUGIN 1.8.0 build on May 31 2011 18:26:37.
File is seekable
specific info size is: 2
specific info size is: 32
BLN_MAD-MMCODECS_AACD_ARM_03.05.00  build on Nov 25 2009 15:00:47.
MFW_GST_AAC_PLUGIN 1.8.0 build on May 31 2011 18:26:24.
MPEG4_ASP_D_01.02.01  build on Sep 27 2009 11:03:16.
MFW_GST_MPEG4ASP_DECODER_PLUGIN 1.8.0 build on May 31 2011 18:26:33.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs
successfully seek audio the track 1
successfully seek video the track 0
[V4L Update Display]: left=0, top=0, width=320, height=240

(totem:925): GStreamer-CRITICAL **: gst_structure_set_value: assertion `IS_MUTABLE (structure)' failed
>>V4L_SINK: Actually buffer status:
        hardware buffer : 7
        software buffer : 0
xcontext: width=320, height=240
>>V4L_SINK: Set max lateness = 2000000000.
DAC underflow detected
DAC overflow detected

...

< here it played a 3min mp4 encoded video, but only audio working>

...


Total rendered:0
>>V4L finalize: class finalized.
MPEG4PARSER_06.01.08  build on Mar  3 2010 17:08:43.
MFW_GST_MP4_PARSER_PLUGIN 1.8.0 build on May 31 2011 18:26:37.
File is seekable
specific info size is: 2
specific info size is: 32
BLN_MAD-MMCODECS_AACD_ARM_03.05.00  build on Nov 25 2009 15:00:47.
MFW_GST_AAC_PLUGIN 1.8.0 build on May 31 2011 18:26:24.
MPEG4_ASP_D_01.02.01  build on Sep 27 2009 11:03:16.
MFW_GST_MPEG4ASP_DECODER_PLUGIN 1.8.0 build on May 31 2011 18:26:33.
IRQ 4/MXS DAC/ADC HP SHORT: IRQF_DISABLED is not guaranteed on shared IRQs
MFW_GST_V4LSINK_PLUGIN 1.8.0 build on May 31 2011 18:26:42.
successfully seek audio the track 1
successfully seek video the track 0
[V4L Update Display]: left=0, top=0, width=320, height=240

(totem:925): GStreamer-CRITICAL **: gst_structure_set_value: assertion `IS_MUTABLE (structure)' failed
>>V4L_SINK: Actually buffer status:
        hardware buffer : 7
        software buffer : 0
xcontext: width=320, height=240
>>V4L_SINK: Set max lateness = 2000000000.

 

  Waiting for your reply....

  Daniel.

0 Kudos
Reply

1,871 Views
daiane_angolini
NXP Employee
NXP Employee
Open totem from some terminal and copy here log you get.
0 Kudos
Reply

1,871 Views
danix
Contributor III

anybody there?... please help. I couldn't solve this.

 

Thanks in advance

0 Kudos
Reply