Unable to mount root fs on unknown-block(0,0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Unable to mount root fs on unknown-block(0,0)

2,024 次查看
layleon
Contributor III

 

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 5.4.47-2.2.0+g5ec03d06f54e (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Tue Nov 17 07:39:15 UTC 2020
[    0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
[    0.000000] CPU: div instructions available: patching division code
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] Reserved memory: incorrect alignment of CMA region
[    0.000000] OF: reserved mem: node linux,cma compatible matching fail
[    0.000000] cma: Reserved 32 MiB at 0x8e000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.0 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 15 pages/cpu s32076 r8192 d21172 u61440
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 56768
[    0.000000] Kernel command line: console=ttymxc0,115200 ubi.mtd=nandrootfs root=ubi0:rootfs rootfstype=ubifs mtdparts=gpmi-nand:64m(nandboot),16m(nandkernel),16m(nanddtb),16m(nandtee),-(nandrootfs)
[    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 174664K/229376K available (12288K kernel code, 576K rwdata, 4272K rodata, 1024K init, 433K bss, 21944K reserved, 32768K cma-reserved, 0K highmem)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[    0.000000]  Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] random: get_random_bytes called from start_kernel+0x2c8/0x488 with crng_init=0
[    0.000000] Switching to timer-based delay loop, resolution 41ns
[    0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[    0.000055] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[    0.002933] Console: colour dummy device 80x30
[    0.003005] Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
[    0.003040] pid_max: default: 32768 minimum: 301
[    0.003427] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.003462] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[    0.005191] CPU: Testing write buffer coherency: ok
[    0.005929] CPU0: update cpu_capacity 1024
[    0.005963] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.060598] Setting up static identity map for 0x80100000 - 0x80100060
[    0.080573] rcu: Hierarchical SRCU implementation.
[    0.120753] smp: Bringing up secondary CPUs ...
[    0.120787] smp: Brought up 1 node, 1 CPU
[    0.120809] SMP: Total of 1 processors activated (48.00 BogoMIPS).
[    0.120828] CPU: All CPU(s) started in SVC mode.
[    0.121719] devtmpfs: initialized
[    0.141311] VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
[    0.142301] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.142352] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[    0.145277] pinctrl core: initialized pinctrl subsystem
[    0.147783] NET: Registered protocol family 16
[    0.168243] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.171037] cpuidle: using governor menu
[    0.189604] vdd3p0: supplied by regulator-dummy
[    0.190989] cpu: supplied by regulator-dummy
[    0.192464] vddsoc: supplied by regulator-dummy
[    0.214119] No ATAGs?
[    0.214259] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.214295] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.218574] imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[    0.221421] imx mu driver is registered.
[    0.222565] imx rpmsg driver is registered.
[    0.308053] vgaarb: loaded
[    0.309996] SCSI subsystem initialized
[    0.313269] usbcore: registered new interface driver usbfs
[    0.313409] usbcore: registered new interface driver hub
[    0.313650] usbcore: registered new device driver usb
[    0.316976] i2c i2c-0: IMX I2C adapter registered
[    0.318724] i2c i2c-1: IMX I2C adapter registered
[    0.319577] mc: Linux media interface: v0.10
[    0.319696] videodev: Linux video capture interface: v2.00
[    0.319839] pps_core: LinuxPPS API ver. 1 registered
[    0.319860] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.319938] PTP clock support registered
[    0.323020] MIPI CSI2 driver module loaded
[    0.323155] Advanced Linux Sound Architecture Driver Initialized.
[    0.324981] Bluetooth: Core ver 2.22
[    0.325115] NET: Registered protocol family 31
[    0.325136] Bluetooth: HCI device and connection manager initialized
[    0.325173] Bluetooth: HCI socket layer initialized
[    0.325200] Bluetooth: L2CAP socket layer initialized
[    0.325257] Bluetooth: SCO socket layer initialized
[    0.326494] clocksource: Switched to clocksource mxc_timer1
[    0.326946] VFS: Disk quotas dquot_6.6.0
[    0.327154] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.350670] thermal_sys: Registered thermal governor 'step_wise'
[    0.351325] NET: Registered protocol family 2
[    0.352753] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[    0.352843] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear)
[    0.352916] TCP bind hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.353006] TCP: Hash tables configured (established 2048 bind 2048)
[    0.353226] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
[    0.353295] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
[    0.353712] NET: Registered protocol family 1
[    0.385259] RPC: Registered named UNIX socket transport module.
[    0.385292] RPC: Registered udp transport module.
[    0.385310] RPC: Registered tcp transport module.
[    0.385326] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.396819] PCI: CLS 0 bytes, default 64
[    0.398407] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 5 counters available
[    0.400840] OPTEE busfreq Supported
[    0.401286] Bus freq driver module loaded
[    0.403741] Initialise system trusted keyrings
[    0.404321] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[    0.432108] NFS: Registering the id_resolver key type
[    0.432185] Key type id_resolver registered
[    0.432205] Key type id_legacy registered
[    0.432311] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.433570] fuse: init (API version 7.31)
[    0.521631] Key type asymmetric registered
[    0.521667] Asymmetric key parser 'x509' registered
[    0.521735] io scheduler mq-deadline registered
[    0.521754] io scheduler kyber registered
[    0.542039] pwm-backlight backlight-display: backlight-display supply power not found, using dummy regulator
[    0.550354] mxsfb 21c8000.lcdif: 21c8000.lcdif supply lcd not found, using dummy regulator
[    0.550693] cma: cma_alloc: alloc failed, req-size: 8192 pages, ret: -12
[    0.550730] mxsfb 21c8000.lcdif: Unable to allocate framebuffer memory
[    0.550758] mxsfb 21c8000.lcdif: Failed to initialize fbinfo: -12
[    0.551129] mxsfb: probe of 21c8000.lcdif failed with error -12
[    0.560787] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[    0.560830] imx-sdma 20ec000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin
[    0.565222] mxs-dma 1804000.dma-apbh: initialized
[    0.578162] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 22, base_baud = 5000000) is a IMX
[    1.326193] printk: console [ttymxc0] enabled
[    1.333010] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 66, base_baud = 5000000) is a IMX
[    1.345272] imx sema4 driver is registered.
[    1.388106] brd: module loaded
[    1.412129] loop: module loaded
[    1.418298] imx ahci driver is registered.
[    1.428660] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xda
[    1.435066] nand: Micron MT29F2G08ABAEAWP
[    1.439186] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[    1.448042] Bad block table found at page 131008, version 0x01
[    1.454221] Bad block table found at page 130944, version 0x01
[    1.460588] 5 cmdlinepart partitions found on MTD device gpmi-nand
[    1.466865] Creating 5 MTD partitions on "gpmi-nand":
[    1.471964] 0x000000000000-0x000004000000 : "nandboot"
[    1.488530] 0x000004000000-0x000005000000 : "nandkernel"
[    1.508494] 0x000005000000-0x000006000000 : "nanddtb"
[    1.528485] 0x000006000000-0x000007000000 : "nandtee"
[    1.548501] 0x000007000000-0x000010000000 : "nandrootfs"
[    1.568549] gpmi-nand 1806000.gpmi-nand: driver registered.
[    1.578799] gpio@0 enforce active low on chipselect handle
[    1.589245] libphy: Fixed MDIO Bus: probed
[    1.594764] CAN device driver interface
[    1.603738] pps pps0: new PPS source ptp0
[    1.608820] fec 20b4000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    1.615595] fec 20b4000.ethernet: Using random MAC address: 52:9f:6c:9f:86:74
[    1.623686] libphy: fec_enet_mii_bus: probed
[    1.628333] mdio_bus 20b4000.ethernet-1: MDIO device at address 2 is missing.
[    1.635715] mdio_bus 20b4000.ethernet-1: MDIO device at address 1 is missing.
[    1.644496] fec 20b4000.ethernet eth0: registered PHC device 0
[    1.653481] pps pps1: new PPS source ptp1
[    1.658661] fec 2188000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[    1.665446] fec 2188000.ethernet: Using random MAC address: 06:c4:ad:fa:fc:9d
[    1.674780] fec 2188000.ethernet eth1: registered PHC device 1
[    1.681411] e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
[    1.687360] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    1.694610] usbcore: registered new interface driver r8152
[    1.700364] usbcore: registered new interface driver lan78xx
[    1.706174] usbcore: registered new interface driver asix
[    1.711770] usbcore: registered new interface driver ax88179_178a
[    1.718039] usbcore: registered new interface driver cdc_ether
[    1.724042] usbcore: registered new interface driver smsc95xx
[    1.729974] usbcore: registered new interface driver net1080
[    1.735748] usbcore: registered new interface driver cdc_subset
[    1.741839] usbcore: registered new interface driver zaurus
[    1.747591] usbcore: registered new interface driver MOSCHIP usb-ethernet driver
[    1.755158] usbcore: registered new interface driver cdc_ncm
[    1.760898] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[    1.767610] ehci-pci: EHCI PCI platform driver
[    1.772234] ehci-mxc: Freescale On-Chip EHCI Host driver
[    1.778529] usbcore: registered new interface driver usb-storage
[    1.789068] imx_usb 2184000.usb: No over current polarity defined
[    1.795367] imx_usb 2184000.usb: 2184000.usb supply vbus not found, using dummy regulator
[    1.831832] imx_usb 2184200.usb: 2184200.usb supply vbus not found, using dummy regulator
[    1.844884] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    1.849960] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[    1.886592] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    1.892486] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[    1.900869] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    1.908175] usb usb1: Product: EHCI Host Controller
[    1.913090] usb usb1: Manufacturer: Linux 5.4.47-2.2.0+g5ec03d06f54e ehci_hcd
[    1.920298] usb usb1: SerialNumber: ci_hdrc.1
[    1.926179] hub 1-0:1.0: USB hub found
[    1.930239] hub 1-0:1.0: 1 port detected
[    1.950180] input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
[    1.966387] input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input1
[    1.979642] read sensor who am i (0xfffffffa)error !
[    1.984698] fxls8471: probe of 0-001e failed with error -22
[    1.995726] snvs_rtc 20cc000.snvs:snvs-rtc-lp: registered as rtc0
[    2.002422] i2c /dev entries driver
[    2.009931] pxp-v4l2 pxp_v4l2: initialized
[    2.015174] syscon-poweroff 20cc000.snvs:snvs-poweroff: pm_power_off already claimed (ptrval) psci_sys_poweroff
[    2.025462] syscon-poweroff: probe of 20cc000.snvs:snvs-poweroff failed with error -16
[    2.035321] mag3110 0-000e: 0-000e supply vdd not found, using dummy regulator
[    2.043720] mag3110 0-000e: 0-000e supply vddio not found, using dummy regulator
[    2.051595] mag3110 0-000e: check mag3110 chip ID
[    2.056807] mag3110 0-000e: read chip ID 0xfffffffa is not equal to 0xc4!
[    2.063942] mag3110: probe of 0-000e failed with error -22
[    2.072809] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[    2.080562] Bluetooth: HCI UART driver ver 2.3
[    2.085064] Bluetooth: HCI UART protocol H4 registered
[    2.090540] Bluetooth: HCI UART protocol BCSP registered
[    2.095993] Bluetooth: HCI UART protocol LL registered
[    2.101374] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    2.107883] Bluetooth: HCI UART protocol Marvell registered
[    2.113644] usbcore: registered new interface driver btusb
[    2.121121] sdhci: Secure Digital Host Controller Interface driver
[    2.127444] sdhci: Copyright(c) Pierre Ossman
[    2.131827] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.140630] sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
[    2.176504] random: fast init done
[    2.193468] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[    2.204305] caam 2140000.caam: device ID = 0x0a16030000000000 (Era 8)
[    2.210933] caam 2140000.caam: job rings = 2, qi = 0
[    2.246929] caam algorithms registered in /proc/crypto
[    2.256409] caam 2140000.caam: caam pkc algorithms registered in /proc/crypto
[    2.267052] caam_jr 2142000.jr1: registering rng-caam
[    2.272594] Device caam-keygen registered
[    2.287975] caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
[    2.298128] usbcore: registered new interface driver usbhid
[    2.303748] usbhid: USB HID core driver
[    2.314181] optee: probing for conduit method from DT.
[    2.319508] optee: revision 3.10 (b3914e54)
[    2.320347] optee: dynamic shared memory is enabled
[    2.330818] optee: initialized driver
[    2.358315] fsl-sai 202c000.sai: failed to get mclk0 clock: -2
[    2.376343] debugfs: Directory '202c000.sai' with parent 'wm8960-audio' already present!
[    2.385201] imx-wm8960 sound-wm8960: wm8960-hifi <-> 202c000.sai mapping ok
[    2.393667] imx-wm8960 sound-wm8960: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
[    2.401607] imx-wm8960 sound-wm8960: wm8960-hifi <-> 202c000.sai mapping ok
[    2.545105] NET: Registered protocol family 26
[    2.551427] NET: Registered protocol family 10
[    2.568775] Segment Routing with IPv6
[    2.572687] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    2.580492] NET: Registered protocol family 17
[    2.585014] can: controller area network core (rev 20170425 abi 9)
[    2.591619] NET: Registered protocol family 29
[    2.596116] can: raw protocol (rev 20170425)
[    2.600490] can: broadcast manager protocol (rev 20170425 t)
[    2.606204] can: netlink gateway (rev 20190810) max_hops=1
[    2.612368] Bluetooth: RFCOMM TTY layer initialized
[    2.617565] Bluetooth: RFCOMM socket layer initialized
[    2.622800] Bluetooth: RFCOMM ver 1.11
[    2.626681] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    2.632028] Bluetooth: BNEP filters: protocol multicast
[    2.637355] Bluetooth: BNEP socket layer initialized
[    2.642353] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    2.648440] Bluetooth: HIDP socket layer initialized
[    2.653548] lib80211: common routines for IEEE802.11 drivers
[    2.659425] Key type dns_resolver registered
[    2.690405] Registering SWP/SWPB emulation handler
[    2.695813] Loading compiled-in X.509 certificates
[    2.742233] regulator-can-3v3 GPIO handle specifies active low - ignored
[    2.757605] imx_thermal tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C
[    2.768258] ubi0: default fastmap pool size: 55
[    2.772829] ubi0: default fastmap WL pool size: 27
[    2.777803] ubi0: attaching mtd4
[    3.425226] ubi0: scanning is finished
[    3.441346] ubi0: attached mtd4 (name "nandrootfs", size 144 MiB)
[    3.447979] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[    3.455107] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 2048
[    3.461975] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[    3.469045] ubi0: good PEBs: 1148, bad PEBs: 4, corrupted PEBs: 0
[    3.475161] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[    3.482442] ubi0: max/mean erase counter: 2/1, WL threshold: 4096, image sequence number: 1745808277
[    3.491667] ubi0: available PEBs: 0, total reserved PEBs: 1148, PEBs reserved for bad PEB handling: 36
[    3.501053] ubi0: background thread "ubi_bgt0d" started, PID 141
[    3.507696] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:05:56 UTC (356)
[    3.517510] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    3.528648] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    3.535469] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    3.544584] ALSA device list:
[    3.547760]   #0: wm8960-audio
[    3.551357] VFS: Cannot open root device "ubi0:rootfs" or unknown-block(0,0): error -19
[    3.559621] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[    3.567787] Please append a correct "root=" boot option; here are the available partitions:
[    3.576176] 0100           65536 ram0
[    3.576181]  (driver?)
[    3.582517] 0101           65536 ram1
[    3.582523]  (driver?)
[    3.588748] 0102           65536 ram2
[    3.588753]  (driver?)
[    3.594885] 0103           65536 ram3
[    3.594889]  (driver?)
[    3.601203] 0104           65536 ram4
[    3.601211]  (driver?)
[    3.607424] 0105           65536 ram5
[    3.607429]  (driver?)
[    3.613561] 0106           65536 ram6
[    3.613566]  (driver?)
[    3.619784] 0107           65536 ram7
[    3.619790]  (driver?)
[    3.625917] 0108           65536 ram8
[    3.625921]  (driver?)
[    3.632131] 0109           65536 ram9
[    3.632138]  (driver?)
[    3.638302] 010a           65536 ram10
[    3.638306]  (driver?)
[    3.644519] 010b           65536 ram11
[    3.644523]  (driver?)
[    3.650768] 010c           65536 ram12
[    3.650772]  (driver?)
[    3.657049] 010d           65536 ram13
[    3.657055]  (driver?)
[    3.663270] 010e           65536 ram14
[    3.663275]  (driver?)
[    3.669525] 010f           65536 ram15
[    3.669530]  (driver?)
[    3.675752] 1f00           65536 mtdblock0
[    3.675758]  (driver?)
[    3.682395] 1f01           16384 mtdblock1
[    3.682400]  (driver?)
[    3.689036] 1f02           16384 mtdblock2
[    3.689040]  (driver?)
[    3.695601] 1f03           16384 mtdblock3
[    3.695607]  (driver?)
[    3.702207] 1f04          147456 mtdblock4
[    3.702211]  (driver?)
[    3.708840] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[    3.717138] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---

 

I don't know how to fix it....

0 项奖励
回复
3 回复数

2,005 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Layleon,

   From logs, it seems that linux CMA size caused the issue.

   So you can try to change cma size according to steps of the link.

https://github.com/alliedvision/documentation/wiki/Changing-memory-size-reserved-for-CMA

 

Have a nice day!

B.R,

weidong

0 项奖励
回复

1,993 次查看
layleon
Contributor III

But now the CMA is only 32MB(headless system) and still can't mount the file system. How much should this be?

0 项奖励
回复

2,019 次查看
layleon
Contributor III

Yocto core-image-minimal clean image

0 项奖励
回复