Unable to handle kernel paging request at virtual address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to handle kernel paging request at virtual address

Jump to solution
4,902 Views
steven1758
Contributor II

Hi

I am using the imx-android-13.4.1 code. after burn to my board ,It will suddenly

give the Unable to handle kernel paging request at virtual address error then crash. :  (

Here is the information:

active wake lock PowerManagerService

request_suspend_state: wakeup (3->0) at 178405733691 (2013-07-09 10:09:59.364397999 UTC)

PHY: 1:05 - Link is Up - 1000/Full

mmc0: Starting deferred resume

mmc0: Deferred resume completed

Unable to handle kernel paging request at virtual address 9fed28f0

pgd = c0004000

[9fed28f0] *pgd=00000000

Internal error: Oops: 805 [#1] PREEMPT SMP

Modules linked in:

CPU: 1    Not tainted  (3.0.35-05524-g8513494-dirty #5)

Any advice will be appreciate .

Thanks

Labels (2)
0 Kudos
Reply
1 Solution
3,604 Views
steven1758
Contributor II

It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )

View solution in original post

0 Kudos
Reply
1 Reply
3,605 Views
steven1758
Contributor II

It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )

0 Kudos
Reply