Unable to handle kernel paging request at virtual address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to handle kernel paging request at virtual address

ソリューションへジャンプ
4,865件の閲覧回数
steven1758
Contributor II

Hi

I am using the imx-android-13.4.1 code. after burn to my board ,It will suddenly

give the Unable to handle kernel paging request at virtual address error then crash. :  (

Here is the information:

active wake lock PowerManagerService

request_suspend_state: wakeup (3->0) at 178405733691 (2013-07-09 10:09:59.364397999 UTC)

PHY: 1:05 - Link is Up - 1000/Full

mmc0: Starting deferred resume

mmc0: Deferred resume completed

Unable to handle kernel paging request at virtual address 9fed28f0

pgd = c0004000

[9fed28f0] *pgd=00000000

Internal error: Oops: 805 [#1] PREEMPT SMP

Modules linked in:

CPU: 1    Not tainted  (3.0.35-05524-g8513494-dirty #5)

Any advice will be appreciate .

Thanks

ラベル(2)
0 件の賞賛
返信
1 解決策
3,567件の閲覧回数
steven1758
Contributor II

It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,568件の閲覧回数
steven1758
Contributor II

It is like that it is about the temperature after let the IMX6Q cool this problem like have solved . : )

0 件の賞賛
返信