Unable to handle kernel NULL pointer dereference at virtual address IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to handle kernel NULL pointer dereference at virtual address IMX6

ソリューションへジャンプ
29,003件の閲覧回数
alokkumar
Contributor III

Dear All,

I have been facing some issue with stability of iMX6 build provided by timesys. I am using boundary devices board.

I am decoding 1080P RTSP streaming 60 fps resolution is little scaled down.

Along with QT weather app and  a ticker. I am seeing something crashes with in ~ 24 hours. Are there any ways where I can reduce the  crashes.

VS1 created. in fmt[NV12] win(0,0-1920,1080:1920x1080) out win(485,0-1925,960:1440x960)

set deinterlace mode 0

cooling: cpu cur freq is 792000000

cooling: cpu max freq set to 396000000

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = 80004000

[00000000] *pgd=00000000

Internal error: Oops: 17 [#1] PREEMPT SMP

Modules linked in: mxc_v4l2_capture ipu_fg_overlay_sdc ipu_csi_enc ipu_prp_enc ipu_still ipu_bg_overlay_sdc ov5642_camera camera_sensor_clock galcore

CPU: 0    Not tainted  (3.0.35-ts-armv7l #1)

PC is at __wake_up_common+0x28/0x90

LR is at __wake_up+0x3c/0x50

pc : [<80066bcc>]    lr : [<80067398>]    psr: a00f0093

sp : bfec3c40  ip : 00000000  fp : bfec3c6c

r10: 00000003  r9 : 00000000  r8 : 00000000

r7 : bfb5f0ac  r6 : 00000000  r5 : 600f0013  r4 : bfb5f0a4

r3 : 00000000  r2 : 00000001  r1 : 00000003  r0 : bfb5f0a4

Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 4a01c04a  DAC: 00000015

Process ipu1_task (pid: 372, stack limit = 0xbfec22f0)

Stack: (0xbfec3c40 to 0xbfec4000)

3c40: 00000000 00000001 00000000 bfb5f0a4 600f0013 00000000 00000001 00000003

3c60: 00200200 00100100 bfec3c94 80067398 00000000 bfb5ee00 bfb5ee00 bfb5ee00

3c80: 00000001 bfb5f08c bfec3f84 00000000 00000000 803b76b4 00000000 00000000

3ca0: 8c008f40 bfc027e0 bfec2000 bfc02f20 00000000 bfb63040 80525840 bfec3cfc

3cc0: 8003bf40 bfec3cdc 80521648 80521688 600f0013 00000001 00000000 00000094

3ce0: 00000000 bfb5ee00 bfec3f84 00000000 00200200 00100100 00000000 803b8258

3d00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000002

3d20: 00000000 bfec2000 00000001 00000001 00000000 00000780 00000440 3231564e

3d40: 000003b0 00000000 000003d0 00000438 18c00000 00000000 00000000 00000780

3d60: 00000438 50424752 00000000 000004a8 00000000 000002d8 000003c0 157e9000

3d80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

3da0: 00000000 00000000 00000000 00000000 00000000 00000000 000003f2 bfdeac00

3dc0: bfdeb000 0016c192 00000780 00000440 3231564e 00000000 00000000 000003d0

3de0: 00000438 18c00000 00000000 00000000 00000780 00000438 50424752 00000000

3e00: 000001e8 00000000 000002d8 000003c0 157e9000 00000000 00000000 00000000

3e20: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

3e40: 00000000 00000000 00000000 000003f2 bfdeac00 bfdeba00 0016c191 00000001

3e60: 00000000 00000001 00000000 00000000 2e7127b2 bfec3f9c bfc027e0 bfec2000

3e80: 00000001 bfc02974 ffff8b75 bffd1700 bfec3f14 8006e604 8c01025c bfec3f9c

3ea0: 00002475 00000000 00000001 bfec2000 312297ca 8003bf40 00002475 8c01025c

3ec0: 8003bf40 00000001 00000002 bffd1700 8073d7cc ffffffff bffac000 00000002

3ee0: 00000000 80092c30 00000000 00000000 00000001 bffac01c bfc027e0 bfec2000

3f00: bff8e0a0 80092c54 8c010f40 bfc027e0 bfec3fc4 80521648 bfec3f9c bff8c000

3f20: bfec3f44 8006a65c 000f4240 00000000 00000001 00000000 312297ca 00000000

3f40: 8003bf40 8003bf40 8003b1b4 8003bf40 00000000 bff8be48 8006fc18 00000001

3f60: bff8be54 00000000 00000000 00000003 bfec3fa4 80066bf4 bfd72c9c 00000000

3f80: 00000000 00000000 bfc027e0 8008dd18 bfec3f90 bfec3f90 00000031 00000001

3fa0: bfec3fc4 bff8be38 80760cec 803b817c 00000013 00000000 00000000 00000000

3fc0: 00000000 8008d6f4 80043a24 00000000 80760cec 00000000 00000000 00000000

3fe0: bfec3fe0 bfec3fe0 bff8be38 8008d674 80043a24 80043a24 00000000 00000000

[<80066bcc>] (__wake_up_common+0x28/0x90) from [<80067398>] (__wake_up+0x3c/0x50)

[<80067398>] (__wake_up+0x3c/0x50) from [<803b76b4>] (get_res_do_task+0x10c/0x584)

[<803b76b4>] (get_res_do_task+0x10c/0x584) from [<803b8258>] (ipu_task_thread+0xdc/0xaf0)

[<803b8258>] (ipu_task_thread+0xdc/0xaf0) from [<8008d6f4>] (kthread+0x80/0x88)

[<8008d6f4>] (kthread+0x80/0x88) from [<80043a24>] (kernel_thread_exit+0x0/0x8)

Code: e1a08003 e5b7c008 e59b9004 e157000c (e41c400c)

---[ end trace 243e3e064b4a65aa ]---

note: ipu1_task[372] exited with preempt_count 1

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = 80004000

Any thoughts will be appreciated.

ラベル(4)
0 件の賞賛
返信
1 解決策
19,448件の閲覧回数
LeonardoSandova
Specialist I

Alok, could you take a look to this thread and see if it is helpful:

GStreamer crashing on i.MX6 (Boundary Devices Nitrogen6x)

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
10 返答(返信)
19,448件の閲覧回数
timothybean
Contributor IV

Alok,

Did this answer fix your issue? I just had the same crash and had never seen it before today.

Thanks

Tim

0 件の賞賛
返信
19,448件の閲覧回数
nickfahrner
Contributor I

Timothy,

I too saw a similar crash for the first time this morning on a kernel that I have been successfully using for a week, however the CPU I am using is the Armada 510.

Nick

0 件の賞賛
返信
19,448件の閲覧回数
timothybean
Contributor IV

Must be the full moon.

I have been using this kernel for a month at least. Now, I have seen this happen a few times in the past couple of days. Although, I did just change my design to boot from a initramfs ram disk instead. Not sure if that has something to do with it or not. It would be nice if I could confirm that the linked to patch does actually work. It seems that this also screws up my video decoding and need to reboot to recover.

I am posting my full output if someone from Freescale can look at this. Nitrogen6X board, BSP 1.1.1, 3.0.35 kernel.

U: 0Tainted: G  D  (3.0.35-g0642749-dirty #205)

PC is at __wake_up_common+0x28/0x90

LR is at __wake_up+0x3c/0x50

pc : [<80064904>]lr : [<80064e74>]psr: a0000193

sp : bf80dc40  ip : 00000000  fp : bf80dc6c

r10: 00000003  r9 : 00000000  r8 : 00000000

r7 : b2da60ac  r6 : 00000000  r5 : 60000113  r4 : b2da60a4

r3 : 00000000  r2 : 00000001  r1 : 00000003  r0 : b2da60a4

Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 42fe804a  DAC: 00000015

Process ipu1_task (pid: 400, stack limit = 0xbf80c2f0)

Stack: (0xbf80dc40 to 0xbf80e000)

dc40: 00000096 00000001 00000000 b2da60a4 60000113 00000000 00000001 00000003

dc60: 00200200 00100100 bf80dc94 80064e74 00000000 00200200 00100100 b2da7600

dc80: 00000001 b2da608c bf80df84 00000000 00000000 803c0e74 80729cc0 80040834

dca0: ffffffff f2a00100 00000096 00000002 00000001 8003f9cc 80791a78 60000013

dcc0: 8075c9e8 00000000 00000094 60000013 b2da7600 00000001 00000000 00000094

dce0: 00000000 b2da7600 bf80df84 00000000 00200200 00100100 00000000 803c1a14

dd00: 00000000 0000001e bfff2600 00000000 bc02eff0 bfff2600 bc02e000 00000002

dd20: 00000000 bf80c000 00000001 00000001 bfff2600 00000500 000002d0 3231564e

dd40: 00000270 00000000 00000290 000002d0 17c00000 00000000 00000000 00000500

dd60: 000002d0 50424752 00000000 00000270 00000000 00000290 000002d0 15800000

dd80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

dda0: 00000000 00000000 00000000 00000000 00000000 00000000 000003f2 b301fe00

ddc0: b2f46800 0166d022 00000500 000002d0 3231564e 00000000 00000000 00000290

dde0: 000002d0 17c00000 00000000 00000000 00000500 000002d0 50424752 00000000

de00: 00000000 00000000 00000290 000002d0 15800000 00000000 00000000 00000000

de20: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

de40: 00000000 00000000 00000000 000003f2 b301fe00 b2f46000 0166d021 8006c37c

de60: 8c01025c bf80df6c 00000000 00000000 00000001 bf80c000 bf804778 80038f40

de80: 1b7b6f9d bf80deac 0000afc8 8c01025c 80038f40 00000001 00000002 bffd1700

dea0: 00001623 00000000 bfca55f8 8c010f90 1de91c0d bf80dedc 00001623 00000000

dec0: bfca55c0 8c010f90 bfca55c0 8c010f90 8076e42c ffffffff bffac000 00000002

dee0: 00000000 800909b8 00000000 00000001 00000001 bffac01c bfca55c0 bf80c000

df00: bff8e0a0 800909dc 8c010f40 bfca55c0 bf80dfc4 80547750 800381b4 80038f40

df20: 0bfd8000 800e8aa4 0004caa8 00000000 bff9eba0 bf804740 1de91c0d 00000000

df40: 80038f40 80038f40 800381b4 80038f40 bf804740 80073d24 bf804740 80038260

df60: ffffffff 800b6464 00000000 00000001 bf80df70 bf804740 ffffffff 00000001

df80: bff8c000 00000000 bfca55c0 8008ba48 bf80df90 bf80df90 00000031 00000001

dfa0: bf80dfc4 bff8be38 80791a94 803c1938 00000013 00000000 00000000 00000000

dfc0: 00000000 8008b424 80040a64 00000000 80791a94 00000000 00000000 00000000

dfe0: bf80dfe0 bf80dfe0 bff8be38 8008b3a4 80040a64 80040a64 00000000 00000000

[<80064904>] (__wake_up_common+0x28/0x90) from [<80064e74>] (__wake_up+0x3c/0x50)

[<80064e74>] (__wake_up+0x3c/0x50) from [<803c0e74>] (get_res_do_task+0x10c/0x584)

[<803c0e74>] (get_res_do_task+0x10c/0x584) from [<803c1a14>] (ipu_task_thread+0xdc/0xaf0)

[<803c1a14>] (ipu_task_thread+0xdc/0xaf0) from [<8008b424>] (kthread+0x80/0x88)

[<8008b424>] (kthread+0x80/0x88) from [<80040a64>] (kernel_thread_exit+0x0/0x8)

Code: e1a08003 e5b7c008 e59b9004 e157000c (e41c400c)

---[ end trace edef023dbd78fe1b ]---

note: ipu1_task[400] exited with preempt_count 1

mxc_hdmi mxc_hdmi: Read EDID again

mxc_hdmi mxc_hdmi: No modes read from edid

mxc_hdmi mxc_hdmi: create default modelist

mxc_hdmi mxc_hdmi: Read EDID again

mxc_hdmi mxc_hdmi: No modes read from edid

mxc_hdmi mxc_hdmi: create default modelist

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = 80004000

[00000000] *pgd=00000000

Internal error: Oops: 17 [#3] PREEMPT SMP

Modules linked in:

CPU: 0Tainted: G  D  (3.0.35-g0642749-dirty #205)

PC is at __wake_up_common+0x28/0x90

LR is at __wake_up+0x3c/0x50

pc : [<80064904>]lr : [<80064e74>]psr: a0000093

sp : bfca3c40  ip : 00000000  fp : bfca3c6c

r10: 00000003  r9 : 00000000  r8 : 00000000

r7 : b2da7cac  r6 : 00000000  r5 : 60000013  r4 : b2da7ca4

r3 : 00000000  r2 : 00000001  r1 : 00000003  r0 : b2da7ca4

Flags: NzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c53c7d  Table: 42fe804a  DAC: 00000015

Process ipu2_task (pid: 403, stack limit = 0xbfca22f0)

Stack: (0xbfca3c40 to 0xbfca4000)

3c40: 00000096 00000001 00000000 b2da7ca4 60000013 00000000 00000001 00000003

3c60: 00200200 00100100 bfca3c94 80064e74 00000000 00200200 00100100 b2da7e00

3c80: 00000001 b2da7c8c bfca3f84 00000000 00000000 803c0e74 bfca3cd4 8008ba54

3ca0: b2f46b68 8006492c b2f46a48 00000001 00200200 b2f46b6c 60000013 00000000

3cc0: 00000001 00000003 00200200 00100100 bfca3cfc 00000001 00000000 00000094

3ce0: 00000000 b2da7e00 bfca3f84 00000000 00200200 00100100 00000000 803c1a14

3d00: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000002

3d20: 00000000 bfca2000 00000001 00000004 00000000 00000500 000002d0 3231564e

3d40: 00000270 00000000 00000290 000002d0 16200000 00000000 00000000 00000500

3d60: 000002d0 50424752 00000000 00000270 00000000 00000290 000002d0 15b84000

3d80: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

3da0: 00000000 00000000 00000000 00000000 00000000 00000000 000003f2 b2f46a00

3dc0: b2f47200 018a17f2 00000500 000002d0 3231564e 00000000 00000000 00000290

3de0: 000002d0 16200000 00000000 00000000 00000500 000002d0 50424752 00000000

3e00: 00000000 00000000 00000290 000002d0 15b84000 00000000 00000000 00000000

3e20: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

3e40: 00000000 00000000 00000000 000003f2 b2f46a00 b2f46800 018a17f1 00000001

3e60: 00000000 00000000 00000000 bfca3f9c bfca4ae0 8c018f40 8c008f40 bff8c000

3e80: 00000000 8c008f74 bfca3f14 8006c688 8c01825c bfca3f9c bf806b80 00000000

3ea0: 00000002 bfca2000 20000093 80038f40 bffd17c8 bffd179c 00000300 8c01825c

3ec0: 80038f40 00000002 00000002 bffd1780 8076e42c ffffffff bffb4000 00000002

3ee0: 00000000 800909b8 00000000 00000300 00000002 bffb401c bfca4ae0 bfca2000

3f00: bff8ef20 800909dc 8c018f40 bfca4ae0 bfca3fc4 80547750 bfca3f9c 80038f40

3f20: 0bfd8000 800e8aa4 000bb1ab 00000000 bff9f5e0 00000000 1f1663a7 00000000

3f40: 80038f40 80038f40 800381b4 80038f40 bf806b80 80073d24 bf806b80 80038260

3f60: ffffffff 800b6464 00000000 800750e0 bfca3f70 bf806b80 ffffffff 00000001

3f80: bff8c000 00000000 bfca4ae0 8008ba48 bfca3f90 bfca3f90 00000031 00000001

3fa0: bfca3fc4 bff8be38 80791ab8 803c1938 00000013 00000000 00000000 00000000

3fc0: 00000000 8008b424 80040a64 00000000 80791ab8 00000000 00000000 00000000

3fe0: bfca3fe0 bfca3fe0 bff8be38 8008b3a4 80040a64 80040a64 00000000 00000000

[<80064904>] (__wake_up_common+0x28/0x90) from [<80064e74>] (__wake_up+0x3c/0x50)

[<80064e74>] (__wake_up+0x3c/0x50) from [<803c0e74>] (get_res_do_task+0x10c/0x584)

[<803c0e74>] (get_res_do_task+0x10c/0x584) from [<803c1a14>] (ipu_task_thread+0xdc/0xaf0)

[<803c1a14>] (ipu_task_thread+0xdc/0xaf0) from [<8008b424>] (kthread+0x80/0x88)

[<8008b424>] (kthread+0x80/0x88) from [<80040a64>] (kernel_thread_exit+0x0/0x8)

Code: e1a08003 e5b7c008 e59b9004 e157000c (e41c400c)

---[ end trace edef023dbd78fe1c ]---

note: ipu2_task[403] exited with preempt_count 1

mxc_ipu mxc_ipu: ERR: [0xb2da7c00] no-0x18a1890, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1890,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:[0xb2da7c00] no-0x18a1890, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2da7800] no-0x18a1892 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2da6a00] no-0x18a1891 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb2da7c00] no-0x18a18a0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb2da7c00] no-0x18a18a0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18a0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2da6a00] no-0x18a18a2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2da7a00] no-0x18a18a1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fc00] no-0x18a18b0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301fc00] no-0x18a18b0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18b0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2da7c00] no-0x18a18b2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2da7a00] no-0x18a18b1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301e600] no-0x18a18c0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2da7a00] no-0x18a18c2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2da6000] no-0x18a18c1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR: [0xb301e600] no-0x18a18c0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18c0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:[0xb301fe00] no-0x18a18d0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301fe00] no-0x18a18d0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18d0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2da6000] no-0x18a18d2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7000] no-0x18a18d1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301e200] no-0x18a18e0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301e200] no-0x18a18e0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18e0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7000] no-0x18a18e2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7200] no-0x18a18e1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fa00] no-0x18a18f0, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301fa00] no-0x18a18f0, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a18f0,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7200] no-0x18a18f2 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7400] no-0x18a18f1 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fc00] no-0x18a1900, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301fc00] no-0x18a1900, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1900,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7400] no-0x18a1902 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7600] no-0x18a1901 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fc00] no-0x18a1910, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7600] no-0x18a1912 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: [0xb301fc00] no-0x18a1910, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1910,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7800] no-0x18a1911 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fa00] no-0x18a1920, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301fa00] no-0x18a1920, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1920,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7800] no-0x18a1922 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7a00] no-0x18a1921 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301e200] no-0x18a1930, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301e200] no-0x18a1930, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1930,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7a00] no-0x18a1932 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7c00] no-0x18a1931 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301e200] no-0x18a1940, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: [0xb301e200] no-0x18a1940, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1940,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7c00] no-0x18a1942 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee6600] no-0x18a1941 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301fc00] no-0x18a1950, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee6600] no-0x18a1952 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: [0xb301fc00] no-0x18a1950, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1950,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee7e00] no-0x18a1951 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!

mxc_ipu mxc_ipu: ERR:[0xb301e600] no-0x18a1960, split_task timeout,j:1,size:2.

mxc_ipu mxc_ipu: ERR:ipu[0] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR:ipu[1] busy_vf:0, busy_pp:0.

mxc_ipu mxc_ipu: ERR: sp_task[0][0xb2ee7e00] no-0x18a1962 done:0,state:split queue,on_list:1, ipu:0x  (null),timeout!

mxc_ipu mxc_ipu: ERR: [0xb301e600] no-0x18a1960, timeout:2020ms!

mxc_ipu mxc_ipu: ERR: no-0x18a1960,ipu_queue_task err:-110

mxc_v4l2_output mxc_v4l2_output.0: display work fail ret = -110

mxc_ipu mxc_ipu: ERR: sp_task[1][0xb2ee6a00] no-0x18a1961 done:0,state:ok,on_list:0, ipu:0x8078db98,timeout!


0 件の賞賛
返信
14,915件の閲覧回数
billchen
Contributor III

Tim  

    Have you resolved this problem ?

タグ(1)
0 件の賞賛
返信
19,448件の閲覧回数
steven1758
Contributor II

Hi Timothy

I have met this problem too.

Do you have found some answer.  ; )

Thanks

0 件の賞賛
返信
19,448件の閲覧回数
timothybean
Contributor IV

Steven,

Were you able to resolve this issue?

Thanks

Tim

0 件の賞賛
返信
19,448件の閲覧回数
LeonardoSandova
Specialist I

alokkumar please change the post's status as unanswered.

timothybean1, have you dump a core crash and review it with gdb?

0 件の賞賛
返信
19,448件の閲覧回数
timothybean
Contributor IV

Working on it now... I also have Eric Nelson helping me as well. But the more eyes the better.

Tim

0 件の賞賛
返信
19,448件の閲覧回数
timothybean
Contributor IV

Unfortunately, no.

I was hoping that Leonardo or Eric Nelson could help out in figuring out the issue. I really don't have time at this point to upgrade to 4.0.0 because I have to ship unit this week.

Tim

0 件の賞賛
返信
19,449件の閲覧回数
LeonardoSandova
Specialist I

Alok, could you take a look to this thread and see if it is helpful:

GStreamer crashing on i.MX6 (Boundary Devices Nitrogen6x)

Leo

0 件の賞賛
返信