Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)

2,667件の閲覧回数
vincentz63
Contributor IV

I have a custom board with i.MX8Mini and LPDDR4 RAM, connected to a MIPI CSI2 (DPHY) camera streaming 1080p30.

We have a test application based on GStreamer that stops and starts video streaming every few seconds.

the application triggers a crash in the v4l2 driver stack after several cycles. This can range from 50 stop/start cycles to 100s or 1000s.

The callstack is always the same. The crash happens in the vb2_buffer_done(), and we think it may be the call to “atomic_dec(&q->owned_by_drv_count);” in this function that triggers it. For a given image (OS + application), the virtual address is always the same (in the CS below 0x1f8).

Any idea what could be going wrong? Has something like this been reported already?

Nov 11 23:08:48 imx8mmbluebird kernel: Unable to handle kernel NULL pointer dereference at virtual address 00000000000001f8
Nov 11 23:08:48 imx8mmbluebird kernel: Mem abort info:
Nov 11 23:08:48 imx8mmbluebird kernel: ESR = 0x96000006
Nov 11 23:08:48 imx8mmbluebird kernel: Exception class = DABT (current EL), IL = 32 bits
Nov 11 23:08:48 imx8mmbluebird kernel: SET = 0, FnV = 0
Nov 11 23:08:48 imx8mmbluebird kernel: EA = 0, S1PTW = 0
Nov 11 23:08:48 imx8mmbluebird kernel: Data abort info:
Nov 11 23:08:48 imx8mmbluebird kernel: ISV = 0, ISS = 0x00000006
Nov 11 23:08:48 imx8mmbluebird kernel: CM = 0, WnR = 0
Nov 11 23:08:48 imx8mmbluebird kernel: user pgtable: 4k pages, 48-bit VAs, pgdp = 0000000037ca5943
Nov 11 23:08:48 imx8mmbluebird kernel: [00000000000001f8] pgd=000000004e2bc003, pud=000000004e296003, pmd=0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: Internal error: Oops: 96000006 [#1] PREEMPT SMP
Nov 11 23:08:48 imx8mmbluebird kernel: Modules linked in: crc32_ce crct10dif_ce mxc_mipi_csi mx6s_capture gs3470_asl XXXXXXXXXXXXX_camera_mipi overlay galcore(O)
Nov 11 23:08:48 imx8mmbluebird kernel: Process onvif_rtsp_app (pid: 3598, stack limit = 0x0000000097265435)
Nov 11 23:08:48 imx8mmbluebird kernel: CPU: 0 PID: 3598 Comm: XXXXXXXXXXXXX Tainted: G O 4.19.35-1.1.0+g9ec518e5baca #1
Nov 11 23:08:48 imx8mmbluebird kernel: Hardware name: XXXXXXXXXXXXX based on i.MX8MM - rev 6 (Burst) (DT)
Nov 11 23:08:48 imx8mmbluebird kernel: pstate: 20000085 (nzCv daIf -PAN -UAO)
Nov 11 23:08:48 imx8mmbluebird kernel: pc : __ll_sc___cmpxchg_case_acq_4+0x4/0x20
Nov 11 23:08:48 imx8mmbluebird kernel: lr : _raw_spin_lock_irqsave+0x34/0x60
Nov 11 23:08:48 imx8mmbluebird kernel: sp : ffff0000172aba20
Nov 11 23:08:48 imx8mmbluebird kernel: x29: ffff0000172aba20 x28: ffff800013f72300
Nov 11 23:08:48 imx8mmbluebird kernel: x27: ffff00000973b710 x26: ffff00000973b710
Nov 11 23:08:48 imx8mmbluebird kernel: x25: ffff80000ea14bd0 x24: ffff80000ea14930
Nov 11 23:08:48 imx8mmbluebird kernel: x23: 00000000000001f8 x22: 0000000000000007
Nov 11 23:08:48 imx8mmbluebird kernel: x21: 0000000000000000 x20: ffff80000ea14ad8
Nov 11 23:08:48 imx8mmbluebird kernel: x19: 0000000000000080 x18: 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x17: 0000000000000000 x16: 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x15: 0000000000000000 x14: 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x13: 0000000000000000 x12: 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x11: 0000000000000000 x10: 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x9 : 0000000000000000 x8 : 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x7 : 0000000000000200 x6 : 0000000000000000
Nov 11 23:08:48 imx8mmbluebird kernel: x5 : 0000000000000000 x4 : ffff80000ea14c88
Nov 11 23:08:48 imx8mmbluebird kernel: x3 : 00000000000001f8 x2 : 0000000000000001
Nov 11 23:08:48 imx8mmbluebird kernel: x1 : 0000000000000000 x0 : 00000000000001f8
Nov 11 23:08:48 imx8mmbluebird kernel: Call trace:
Nov 11 23:08:48 imx8mmbluebird kernel: __ll_sc___cmpxchg_case_acq_4+0x4/0x20
Nov 11 23:08:48 imx8mmbluebird kernel: vb2_buffer_done+0xa4/0x1b0
Nov 11 23:08:48 imx8mmbluebird kernel: mx6s_stop_streaming+0xbc/0x298 [mx6s_capture]
Nov 11 23:08:48 imx8mmbluebird kernel: __vb2_queue_cancel+0x2c/0x1c8
Nov 11 23:08:48 imx8mmbluebird kernel: vb2_core_streamoff+0x20/0xa8
Nov 11 23:08:48 imx8mmbluebird kernel: vb2_streamoff+0x18/0x60
Nov 11 23:08:48 imx8mmbluebird kernel: mx6s_vidioc_streamoff+0x58/0xc0 [mx6s_capture]
Nov 11 23:08:48 imx8mmbluebird kernel: v4l_streamoff+0x20/0x28
Nov 11 23:08:48 imx8mmbluebird kernel: __video_do_ioctl+0x248/0x498
Nov 11 23:08:48 imx8mmbluebird kernel: video_usercopy+0x268/0x4d0
Nov 11 23:08:48 imx8mmbluebird kernel: video_ioctl2+0x14/0x20
Nov 11 23:08:48 imx8mmbluebird kernel: v4l2_ioctl+0x40/0x118
Nov 11 23:08:48 imx8mmbluebird kernel: do_vfs_ioctl+0xb8/0x890
Nov 11 23:08:48 imx8mmbluebird kernel: ksys_ioctl+0x78/0xa8
Nov 11 23:08:48 imx8mmbluebird kernel: __arm64_sys_ioctl+0x1c/0x28
Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc_common+0x84/0xf0
Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc_handler+0x2c/0x80
Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc+0x8/0xc
Nov 11 23:08:48 imx8mmbluebird kernel: Code: 35ffff91 aa1003e0 d65f03c0 f9800011 (885ffc10)
Nov 11 23:08:48 imx8mmbluebird kernel: ---[ end trace 16bd3712444c4359 ]---

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,550件の閲覧回数
vincentz63
Contributor IV

Hello,

Any progress on this?

Regards,

0 件の賞賛
返信

2,639件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes it looks like a bug I will reported immediately thanks for the catch!.

Regards

0 件の賞賛
返信