Unable to enable Bluetooth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to enable Bluetooth

跳至解决方案
2,240 次查看
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on IMX8QM-MEK platform in Bluetooth. I got following error

mek_8q:/ # cat /sys/class/rfkill/rfkill0/state
1

08-16 10:41:28.795  1768  1768 D bt_upio : is_rfkill_disabled ? [0]
08-16 10:41:28.795  1768  1768 E bt_upio : set_bluetooth_power : open(/sys/class/rfkill/rfkill0/state) for write failed: Permission denied (13)

Thanks & Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
0 项奖励
回复
1 解答
2,163 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,164 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

0 项奖励
回复
2,163 次查看
vinothkumars
Senior Contributor IV

Thank you Ivan for the reply.

Vinoth S,

Regards,
Vinothkumar Sekar
0 项奖励
回复