Unable to enable Bluetooth

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to enable Bluetooth

Jump to solution
2,868 Views
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on IMX8QM-MEK platform in Bluetooth. I got following error

mek_8q:/ # cat /sys/class/rfkill/rfkill0/state
1

08-16 10:41:28.795  1768  1768 D bt_upio : is_rfkill_disabled ? [0]
08-16 10:41:28.795  1768  1768 E bt_upio : set_bluetooth_power : open(/sys/class/rfkill/rfkill0/state) for write failed: Permission denied (13)

Thanks & Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
2,791 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

View solution in original post

0 Kudos
Reply
2 Replies
2,792 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

0 Kudos
Reply
2,791 Views
vinothkumars
Senior Contributor IV

Thank you Ivan for the reply.

Vinoth S,

Regards,
Vinothkumar Sekar
0 Kudos
Reply