Unable to build libdri

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to build libdri

1,666 Views
erice
Contributor I

Hi,

When I run the egl demo program, that is using X11, it is only show a white screen in ltib rootfs. But using the Ubuntu image by Freescale's, it is working normally.

So I think it is a problem of x11 video driver. Then I build the libdri and related libraries. However, we cannot compile the libdri, libdri2... using LTIB, it shows lots of header files are missing.

Which distribution of Linux is prefer for the specified version of LTIB (ltib 3.0.101-4.1.1)?

Labels (2)
0 Kudos
Reply
1 Reply

1,631 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Eric,

Did you try with the latest patch for 3.0.101 that includes the GPU driver and library to 4.6.9p13?

https://www.freescale.com/webapp/Download?colCode=IMX6LXPATCHRN&appType=license&location=null&fasp=1...

Regards

0 Kudos
Reply