Unable to build libdri

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to build libdri

1,678件の閲覧回数
erice
Contributor I

Hi,

When I run the egl demo program, that is using X11, it is only show a white screen in ltib rootfs. But using the Ubuntu image by Freescale's, it is working normally.

So I think it is a problem of x11 video driver. Then I build the libdri and related libraries. However, we cannot compile the libdri, libdri2... using LTIB, it shows lots of header files are missing.

Which distribution of Linux is prefer for the specified version of LTIB (ltib 3.0.101-4.1.1)?

ラベル(2)
0 件の賞賛
返信
1 返信

1,643件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Eric,

Did you try with the latest patch for 3.0.101 that includes the GPU driver and library to 4.6.9p13?

https://www.freescale.com/webapp/Download?colCode=IMX6LXPATCHRN&appType=license&location=null&fasp=1...

Regards

0 件の賞賛
返信