Unable to Connect and share the file using Wi-Fi Direct for IMX8MP board using Realtek(RTL8822BU)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to Connect and share the file using Wi-Fi Direct for IMX8MP board using Realtek(RTL8822BU)

1,223 Views
Yamini
Contributor I

Hi,
I recently worked on IMX8MP Phytec PhyBoard Pollux to bring up Wi-Fi using Realtek Chipset on LINUX Platform, i made the board to act as a Host (Access point) and Station (client) using Hostapd. conf and wpa_supplicant.conf files respectively and can share the internet from IMX8MP Board to external Connected devices(Clients).
Currently, I am working on Wi-Fi Direct sharing (peer-to-peer communication) on IMX8MP Board using Realtek Chipset(RTL8822BU) by using the same wpa_supplicant.conf file and wpa_cli.

 

By using the following commands, I can scan and list out nearby Wi-Fi Direct devices and connect to the particular Wi-Fi device using Wi-Fi Direct(P2P). But, the established connection is getting disconnected within a few seconds and I am unable to share the information/data between two connected devices.

 

p2p_find
p2p_peers
p2p_connect <dev mac Address> <pbc/pin>

 

Here, is the issue I am facing while trying to connect and share the data.

 

> p2p_connect 92:d4:73:d0:95:90 pbc
OK
<3>P2P-FIND-STOPPED 
<3>P2P-GO-NEG-SUCCESS role=client freq=5240 ht40=0 peer_dev=92:d4:73:d0:95:90 peer_iface=92:d4:73:d0:95:90 wps_method=PBC
<3>WPS-PBC-ACTIVE 
<3>CTRL-EVENT-SCAN-STARTED 
<3>CTRL-EVENT-SCAN-RESULTS 
<3>WPS-AP-AVAILABLE 
<3>CTRL-EVENT-SCAN-STARTED 
<3>CTRL-EVENT-SCAN-RESULTS 
<3>WPS-AP-AVAILABLE 
<3>CTRL-EVENT-SCAN-STARTED 
<3>CTRL-EVENT-SCAN-RESULTS 
<3>WPS-AP-AVAILABLE-PBC 
<3>Trying to associate with 92:d4:73:d0:95:90 (SSID='DIRECT-j8-iQOO Z6 Pro' freq=5240 MHz)
<3>Associated with 92:d4:73:d0:95:90
<3>CTRL-EVENT-SUBNET-STATUS-UPDATE status=0
<3>CTRL-EVENT-REGDOM-CHANGE init=COUNTRY_IE type=COUNTRY alpha2=IN
<3>CTRL-EVENT-EAP-STARTED EAP authentication started
<3>CTRL-EVENT-EAP-STATUS status='started' parameter=''
<3>CTRL-EVENT-EAP-PROPOSED-METHOD vendor=14122 method=1
<3>CTRL-EVENT-EAP-STATUS status='accept proposed method' parameter='WSC'
<3>CTRL-EVENT-EAP-METHOD EAP vendor 14122 method 1 (WSC) selected
<3>WPS-CRED-RECEIVED 
<3>WPS-SUCCESS 
<3>P2P-GROUP-FORMATION-SUCCESS 
<3>CTRL-EVENT-EAP-STATUS status='completion' parameter='failure'
<3>CTRL-EVENT-EAP-FAILURE EAP authentication failed
<3>CTRL-EVENT-DISCONNECTED bssid=92:d4:73:d0:95:90 reason=3 locally_generated=1

 

Here, I am attaching the logs of it.

0 Kudos
Reply
1 Reply

1,205 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Yamini!

Thank you for contacting NXP Support!

Sorry, our  source code is for our EVK boards and only works for our Wifi-Modules, and other modules are not implemented.

Please try to use the Phytec source code:

https://www.phytec.eu/en/bsp-download/?bsp=BSP-Android-NXP-i.MX8MP-ALPHA1

If the problem persists try to contact Phytec support.

Best Regards!
Chavira

0 Kudos
Reply