Unable to Boot Container SET1 on IMX8DX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to Boot Container SET1 on IMX8DX

1,752件の閲覧回数
nkhan2
Contributor II

We are unable to boot SET1 container on IMX8DX, however only SET0 container is booting.

Both SET0 and SET1 containers are identical(for testing purposes). Any config required to enable this SET1 container boot?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,709件の閲覧回数
nkhan2
Contributor II

Additional Info :

We are using EMMC boot and below is the layout for reference. Size of each container is 449 KB

pastedImage_1.png

0 件の賞賛
返信

1,709件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nisar,

It is highly dependent on 8DX SOC Version (B0 and C0).

 

For C0, those are the booting scenarios: 

 

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-1342895-323394/pastedImage_2.png

 

So, depending on what partitions are used (boot / user), primary and secondary container set can be set on Boot or USER partitions.

Regards

0 件の賞賛
返信