Udpsink "Internal data flow problem" on MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Udpsink "Internal data flow problem" on MX6

1,373 次查看
RobbieJiang
Contributor IV

Hi,

I'm using the following gstreamer pipeline to stream H.264 video from MX6Q/Linux to PC.

gst-launch -v tvsrc device=/dev/video0 capture-mode=0 ! 'video/x-raw-yuv,format=(fourcc)UYVY,width=720,height=576,framerate=25/1' ! mfw_ipucsc ! 'video/x-raw-yuv,format=(fourcc)I420, width=720,height=576,framerate=25/1'! mfw_deinterlacer ! vpuenc codec=avc   gopsize=2 ! video/x-h264,width=720,height=576 ! rtph264pay mtu=1024 ! udpsink host=192.168.0.68 port=5004

At the end of the output message, I got:

"

WARNING: from element /GstPipeline:pipeline0/GstUDPSink:udpsink0: Internal data flow problem.

Additional debug info:

gstbasesink.c(3626): gst_base_sink_chain_unlocked (): /GstPipeline:pipeline0/GstUDPSink:udpsink0:

Received buffer without a new-segment. Assuming timestamps start from 0.

"

Although the receiver pipeline on host (192.168.0.68) can correctly receive, decode and display the live video,

I am still wondering what "udpsink0: Internal data flow problem" mean.

Is there anything wrong here?

What is the root cause of the udpsink "Internal data flow" problem?

And is it possible to fix it?

Regards,

Robbie

标签 (3)
0 项奖励
回复
2 回复数

1,138 次查看
joanxie
NXP TechSupport
NXP TechSupport

it seems sync issue, try to set sync=true to check if you can stop the warning.

0 项奖励
回复

1,138 次查看
RobbieJiang
Contributor IV

Setting udpsink property 'sync=false' resolved the problem.

The default value of sync property is 'true'.

Guanqiong, thanks for your hints.

0 项奖励
回复