Hi ,the usb gadget unit test fails looking for arcotg_udc.ko in lib/modules ..Is there a seperate way to include this module to run the tests ?
root@freescale /unit_tests$ ./autorun-usb-gadget.sh 10.25.40.189
USB Ethernet Gadget test
Attempting insmod /lib/modules/3.0.35-2508-g54750ff/kernel/drivers/usb/gadget/arcotg_udc.ko
insmod: can't insert '/lib/modules/3.0.35-2508-g54750ff/kernel/drivers/usb/gadget/arcotg_udc.ko': No such file or directory
autorun-usb-gadget.sh: FAIL: insmod returned error
Checking lsmod for the module arcotg_udc
FAIL: module does not appear in lsmod
Module Size Used by
autorun-usb-gadget.sh: Exiting FAIL
Regards
Wnm
Hi wasim
one can use demo images, they have all files in appropriate locations
L3.0.35_4.1.0_DEMO_IMAGE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX
6Solo and i.MX 6Sololite Linux Binary Demo Files
alternatively, one can execute all script commands manually
(finding location arcotg_udc.ko). Also one can check if USB driver is included in
build, check attached Linux Manual sect.34.2.3 Menu Configuration Options
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------