Ubuntu-desktop is needed for GUI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ubuntu-desktop is needed for GUI?

5,015件の閲覧回数
ajayvenkatakris
Contributor II

Hi, 

   I am currently running my IMX6 Sabre auto with the full Ubuntu 14.04 rootfs. Although it is working properly through the serial connection, I am not getting the GUI through HDMI connection. Is the ubuntu-desktop unity required for the GUI to show?

0 件の賞賛
返信
3 返答(返信)

4,809件の閲覧回数
art
NXP Employee
NXP Employee

Also, refer to the attached documents. Hope it will be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,809件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

https://community.nxp.com/docs/DOC-330147 

Hope this information help you.

0 件の賞賛
返信

4,809件の閲覧回数
ajayvenkatakris
Contributor II

Hi,

   I have installed ubuntu-desktop but I am getting an error saying that the system is running on low graphics mode. How do I solve this error?

0 件の賞賛
返信