Uboot cmd usb start error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uboot cmd usb start error

1,481 Views
1282497337
Contributor II

hi community 
      when I use the cmd "usb start" at Uboot stage I got the error line :
starting USB ....... 
USB 0    Port not available .

My Uboot is 2015.04 , the chip is imx6d7c . then what should i do to find this problem
thinks .

Alee

Labels (1)
0 Kudos
Reply
1 Reply

1,344 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alee

one can check hardware using recommendations for usb in

i.MX6 System Development User’s Guide (rev.2, 10/2016)

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

and test with nxp uboot from

uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply