Ubi error during boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ubi error during boot

2,040 Views
pierreq
Contributor I

Hello all,

I try to use Imx287 with nand, i haved build mfg tools un kernel,

I can flash the nand with mfg tools and make ubi fs.

But the kernel can't read the ubifs.

The error is:

0x000001400000-0x000020000000 : "gpmi-nfc-general-use"
UBI: attaching mtd1 to ubi0
UBI: physical eraseblock size: 131072 bytes (128 KiB)
UBI: logical eraseblock size: 126976 bytes
UBI: smallest flash I/O unit: 2048
UBI: VID header offset: 2048 (aligned 2048)
UBI: data offset: 4096
UBI error: ubi_scan_add_used: two LEBs with same sequence number 6
UBI error: ubi_init: cannot attach mtd1

What can i do?

Labels (1)
0 Kudos
Reply
3 Replies

1,965 Views
pierreq
Contributor I

i use ltib with linux 2.6.35

0 Kudos
Reply

1,965 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try to 'flash_eraseall' before (re-)writing your image.

Regards,

Yuri.

0 Kudos
Reply

1,965 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   What Linux BSP is used in the case?

Regards,

Yuri.

0 Kudos
Reply