Uart2 with sdma1 test error in imx8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Uart2 with sdma1 test error in imx8mq

3,320 Views
hongxingyu1982
Contributor III

Hi

Now I test uart2 with sdma1, but when I write character to "dev/ttymxc1" (it is for uart2 device), It report the blew error:

pastedImage_3.png 

Could anyone know this error, and how to fix it ?

BR

0 Kudos
Reply
7 Replies

3,215 Views
hongxingyu1982
Contributor III

HI everyone:

Could anyone can see this issue ? 

Thanks

Br

0 Kudos
Reply

3,215 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hongxing

what bsp used in the case, suggest to try ones from

source.codeaurora.org/external/imx/linux-imx  repository
linux-imx - i.MX Linux kernel 

for uart2 one can check below dts (it can be used by M4)

fsl-imx8mq.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

fsl-imx8mq-evk-root.dts\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,215 Views
hongxingyu1982
Contributor III

HI igor

Any progress ?

//BR

0 Kudos
Reply

3,215 Views
hongxingyu1982
Contributor III

hi igo

Any progress?

BR

0 Kudos
Reply

3,215 Views
hongxingyu1982
Contributor III

Hi igor

Any progress ?

BR

0 Kudos
Reply

3,215 Views
hongxingyu1982
Contributor III

HI igor

If I test the uart2 without sdma1, it is ok.

So the uart2 is ok, maybe the sdma1 is not ok.

So Could you give some supply if is the sdma1 is not ok?

BR

0 Kudos
Reply

3,215 Views
hongxingyu1982
Contributor III

If I test the uart2 without sdma1, it is ok.

So the uart2 is ok, maybe the sdm1 is not ok.

0 Kudos
Reply