UUU tool using UART Port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU tool using UART Port

ソリューションへジャンプ
1,170件の閲覧回数
ahmedmd
Contributor II

Hello Guys,

There is an use case in which I need to flash a Linux BSP on my iMX8QXP board thorough UART port since only that port is available. How do I configure the UUU tool to flash the board using the UART port ?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,157件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,158件の閲覧回数
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

0 件の賞賛
返信