UUU tool using UART Port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

UUU tool using UART Port

跳至解决方案
2,124 次查看
ahmedmd
Contributor II

Hello Guys,

There is an use case in which I need to flash a Linux BSP on my iMX8QXP board thorough UART port since only that port is available. How do I configure the UUU tool to flash the board using the UART port ?

0 项奖励
回复
1 解答
2,111 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,112 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复