UUU tool support for iMX8MP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UUU tool support for iMX8MP

4,501件の閲覧回数
msarwar
Contributor III

Hi guys,

 

I had a look through the UUU config and saw that the iMX8 M Plus is currently not supported by the uuu manufacturing tool. Is this correct ?

(I checked the libuuu config.cpp code in the NXPmicro git repo: https://github.com/NXPmicro/mfgtools/blob/master/libuuu/config.cpp).


I tried to use uuu v1.4.72 with an iMX8MPEVK board with the switches set to serial download mode but uuu didn't recognize any devices. Is there some way to get uuu to work with the imx8mpevk, or some documentation to refer to with more details about this subject ?

 

Thanks

 

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

3,936件の閲覧回数
paulh9898
Contributor I

Will uuu support a iMX8MPlusEVK board, I am using uuu v1.4.224-4-g3903471 to program u-boot into QSPI.

By looking at lsusb I can see the VID/PID is  0403:6011, FT4232H Quad HS USB-UART/FIFO IC.

I am trying to program QSPI using the cmd sudo uuu -b qspi flash.bin. The result is uuu is waiting for a usb device.

By looking at libuuu/config.cpp I dont see that VID/PID listed. Do I need to add a line for this board.

I am plugging in the power supply into PORT0 (J23) and console port into the debug port mini USB

0 件の賞賛
返信

4,494件の閲覧回数
ms_emsys
Contributor I

The modules we use  (DART-MX8M-PLUS) can be flashed with uuu:

 

 

[687443.454421] usb 3-7: new high-speed USB device number 11 using xhci_hcd
[687443.582913] usb 3-7: New USB device found, idVendor=1fc9, idProduct=0146
[687443.582918] usb 3-7: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[687443.582921] usb 3-7: Product: SE Blank 865 
[687443.582924] usb 3-7: Manufacturer: NXP       SemiConductor Inc
[687443.584348] hid-generic 0003:1FC9:0146.0006: hiddev0,hidraw2: USB HID v1.10 Device [NXP       SemiConductor Inc  SE Blank 865  ] on usb-0000:00:14.0-7/input0
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760
 
Connected Known USB Devices
    Path     Chip    Pro     Vid     Pid     BcdVersion
    ==================================================
    3:7  MX865   SDPS:   0x1FC9 0x0146   0x0002

 

 Have you check if a new usb device is detected  by the host (e.g. lsusb/dmesg)?

 

0 件の賞賛
返信

4,481件の閲覧回数
msarwar
Contributor III

Hi @ms_emsys,

I'd expect to see an "SE Blank" device when the iMX 8M EVK board is set to serial download mode too, but I don't get that, just some generic HID device in Windows. Nothing in Linux either.

0 件の賞賛
返信

4,473件の閲覧回数
ms_emsys
Contributor I

I guess your board does not enter SDL mode. Double check the BOOT dip switch and remove the sd card before booting.

What are your settings for SW801 and SW802? SW802 should be D1 OFF D2 ON for SDL mode according to the schematic.

 

0 件の賞賛
返信