USB2.0 Peripheral compliance test i.MX6 Solo OTG port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB2.0 Peripheral compliance test i.MX6 Solo OTG port

1,325 Views
junya
Contributor IV

Hello All,

I want to connect to the host PC using the USB otg port.

But, the host PC don't recognize i.mx6(device).

I understand that connecting a PC and I.MX6 in connector,

USB controller is recognize automatically, is it right?

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

1,111 Views
igorpadykov
NXP Employee
NXP Employee

Hi junya

for PC to be able to recognize i.MX6

i.MX6 should run Linux or put in Serial Downloader

mode. That is it should run some program.

If this is new board one can try to run SDK usb test with jtag:

i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,111 Views
junya
Contributor IV

Thanks for help.

I confirmed that is recognized the i.MX6 in Serial Downloader mode.

Do I need especial software to operate the usb device mode on Linux?

0 Kudos
Reply

1,111 Views
igorpadykov
NXP Employee
NXP Employee

refer to attached docs from imx-test-xx package.

0 Kudos
Reply