USB2.0 Peripheral compliance test i.MX6 Solo OTG port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB2.0 Peripheral compliance test i.MX6 Solo OTG port

1,324件の閲覧回数
junya
Contributor IV

Hello All,

I want to connect to the host PC using the USB otg port.

But, the host PC don't recognize i.mx6(device).

I understand that connecting a PC and I.MX6 in connector,

USB controller is recognize automatically, is it right?

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,110件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi junya

for PC to be able to recognize i.MX6

i.MX6 should run Linux or put in Serial Downloader

mode. That is it should run some program.

If this is new board one can try to run SDK usb test with jtag:

i.MX 6Series Platform SDK

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,110件の閲覧回数
junya
Contributor IV

Thanks for help.

I confirmed that is recognized the i.MX6 in Serial Downloader mode.

Do I need especial software to operate the usb device mode on Linux?

0 件の賞賛
返信

1,110件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

refer to attached docs from imx-test-xx package.

0 件の賞賛
返信