USB supplied while i.MX6 is off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB supplied while i.MX6 is off

ソリューションへジャンプ
3,156件の閲覧回数
electricar
Contributor I

Hello,

am I getting this right, that it's not a problem when the USB ports of the i.MX6 are powered from another device while the i.MX6 is off (not powered)?

Thank you very much in advance.

Kind regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,079件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:

USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,080件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

you are right, i.MX6DQ Datasheet sect.4.2.1 Power-Up Sequence describes:

USB_OTG_VBUS and USB_H1_VBUS are not part of the power supply
sequence and can be powered at any time.

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信