USB gadget zero on i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB gadget zero on i.MX53

Jump to solution
2,533 Views
tzp
Contributor I

Hello dear community!

I am  facing some problems understanding how to write a gadget zero kernel module for the i.MX53.

Can somebody point me to a good source for documentation or some Examples?

Thanks in advance!

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,126 Views
fabio_estevam
NXP Employee
NXP Employee

I grepped the kernel source for "gadget zero":

$ git grep "gadget zero"drivers/usb/core/otg_whitelist.h:/* gadget zero, for testing */

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/pch_udc.c:   /* call gadget zero with setup data received */

drivers/usb/gadget/pxa27x_udc.c:                /* Endpoints for gadget zero */

drivers/usb/misc/usbtest.c:     .name           = "Linux gadget zero",

Not so much of info we can find, but since this is not i.mx related the best place to ask about this topic is the [email protected] mailing list.


View solution in original post

0 Kudos
Reply
2 Replies
2,126 Views
YixingKong
Senior Contributor IV

m_z, please click Correct Answer/Helpful Answer if your question had been answered.

Thanks,

Yixing

0 Kudos
Reply
2,127 Views
fabio_estevam
NXP Employee
NXP Employee

I grepped the kernel source for "gadget zero":

$ git grep "gadget zero"drivers/usb/core/otg_whitelist.h:/* gadget zero, for testing */

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/pch_udc.c:   /* call gadget zero with setup data received */

drivers/usb/gadget/pxa27x_udc.c:                /* Endpoints for gadget zero */

drivers/usb/misc/usbtest.c:     .name           = "Linux gadget zero",

Not so much of info we can find, but since this is not i.mx related the best place to ask about this topic is the [email protected] mailing list.


0 Kudos
Reply