USB gadget zero on i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB gadget zero on i.MX53

ソリューションへジャンプ
2,531件の閲覧回数
tzp
Contributor I

Hello dear community!

I am  facing some problems understanding how to write a gadget zero kernel module for the i.MX53.

Can somebody point me to a good source for documentation or some Examples?

Thanks in advance!

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,124件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I grepped the kernel source for "gadget zero":

$ git grep "gadget zero"drivers/usb/core/otg_whitelist.h:/* gadget zero, for testing */

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/pch_udc.c:   /* call gadget zero with setup data received */

drivers/usb/gadget/pxa27x_udc.c:                /* Endpoints for gadget zero */

drivers/usb/misc/usbtest.c:     .name           = "Linux gadget zero",

Not so much of info we can find, but since this is not i.mx related the best place to ask about this topic is the [email protected] mailing list.


元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,124件の閲覧回数
YixingKong
Senior Contributor IV

m_z, please click Correct Answer/Helpful Answer if your question had been answered.

Thanks,

Yixing

0 件の賞賛
返信
2,125件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

I grepped the kernel source for "gadget zero":

$ git grep "gadget zero"drivers/usb/core/otg_whitelist.h:/* gadget zero, for testing */

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/amd5536udc.c:                /* call gadget zero with setup d

drivers/usb/gadget/pch_udc.c:   /* call gadget zero with setup data received */

drivers/usb/gadget/pxa27x_udc.c:                /* Endpoints for gadget zero */

drivers/usb/misc/usbtest.c:     .name           = "Linux gadget zero",

Not so much of info we can find, but since this is not i.mx related the best place to ask about this topic is the [email protected] mailing list.


0 件の賞賛
返信