USB device mode not working imx6dl-sabresd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB device mode not working imx6dl-sabresd

跳至解决方案
2,203 次查看
winstonjacob
Contributor IV

I am using custom imx6dl board add yocto 4.9.88, my board is having USB OTG, their host mode is properly working, but the device mode not working, please give me the suggestion what modifications I need to do in dts file. Here I attached my dts  file.

Regards

Winston

标签 (3)
0 项奖励
回复
1 解答
2,180 次查看
winstonjacob
Contributor IV

Thanks @igorpadykov , I changed the USB_OTG_ID to high now USB device mode is working properly

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,194 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Winston

 

one can check USB_OTG_ID signal with oscillocope, it should be high or floating in device

mode, also recommended to compare custom board schemiatic usb section with Sabre SD board

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu...

For dts one can look at sect.4.10.2.5 Changing the Controller Operation Mode Linux Manual

included in Documentation

 

Best regards
igor

0 项奖励
回复
2,181 次查看
winstonjacob
Contributor IV

Thanks @igorpadykov , I changed the USB_OTG_ID to high now USB device mode is working properly

0 项奖励
回复