USB device mode not working imx6dl-sabresd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB device mode not working imx6dl-sabresd

ソリューションへジャンプ
2,248件の閲覧回数
winstonjacob
Contributor IV

I am using custom imx6dl board add yocto 4.9.88, my board is having USB OTG, their host mode is properly working, but the device mode not working, please give me the suggestion what modifications I need to do in dts file. Here I attached my dts  file.

Regards

Winston

ラベル(3)
0 件の賞賛
返信
1 解決策
2,225件の閲覧回数
winstonjacob
Contributor IV

Thanks @igorpadykov , I changed the USB_OTG_ID to high now USB device mode is working properly

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,239件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Winston

 

one can check USB_OTG_ID signal with oscillocope, it should be high or floating in device

mode, also recommended to compare custom board schemiatic usb section with Sabre SD board

Design files, including hardware schematics, Gerbers, and OrCAD files for i.MX 6Quad (i.MX 6Dual emu...

For dts one can look at sect.4.10.2.5 Changing the Controller Operation Mode Linux Manual

included in Documentation

 

Best regards
igor

0 件の賞賛
返信
2,226件の閲覧回数
winstonjacob
Contributor IV

Thanks @igorpadykov , I changed the USB_OTG_ID to high now USB device mode is working properly

0 件の賞賛
返信