USB adb enumeration fails when the battery is not fully charged

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB adb enumeration fails when the battery is not fully charged

1,528 次查看
pyh0603
Contributor III

Hello,

Release: android_p11.0.0_2.6.0

Board: i.MX8MQ based custom board

 

When my battery voltage is greater than 8.4V, I can properly enumerate USB ADBs,

When my battery voltage is less than 8.4V, USB adb enumeration fails, and the failure log is as follows:

[ 1283.805549][ T260] type=1400 audit(1722588400.491:39117): avc: denied { read } for comm="Binder:276_2" name="wakeup4" dev="sysfs" ino=27939 scontext=u:r:system_suspend:s0 tcontext=u:object_r:sysfs:s0 tclass=dir permissive=1
[ 1283.841901][ T407] audit: audit_lost=36772 audit_rate_limit=5 audit_backlog_limit=64
[ 1283.842691][ T419] healthd: battery l=67 v=7812 t=36.0 h=2 st=3 c=0 fc=0 cc=32 chg=
[ 1283.842713][ T420] healthd: battery l=67 v=7812 t=36.0 h=2 st=3 c=0 fc=0 cc=32 chg=
[ 1283.850151][ T407] audit: rate limit exceeded
[ 1283.863383][ T420] healthd: battery l=67 v=7812 t=36.0 h=2 st=3 c=0 fc=0 cc=32 chg=

[ 1284.336359][ T5762] android_work: sent uevent USB_STATE=DISCONNECTED
[ 1284.343051][ T5762] usb 1-1: USB disconnect, device number 4
[ 1284.389366][ T1785] read descriptors
[ 1284.393005][ T1785] read strings
[ 1284.880214][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1284.965841][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.021936][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.029293][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.040606][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.047868][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.055181][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.066476][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.081857][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.089353][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.096789][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.180398][ T420] healthd: battery l=67 v=7972 t=36.0 h=2 st=2 c=0 fc=0 cc=32 chg=u
[ 1285.188466][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.190184][ T407] healthd: battery l=67 v=7972 t=36.0 h=2 st=2 c=0 fc=0 cc=32 chg=u
[ 1285.192111][ T419] healthd: battery l=67 v=7972 t=36.0 h=2 st=2 c=0 fc=0 cc=32 chg=u
[ 1285.203213][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.218586][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.225762][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.232956][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.277792][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.285494][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.292969][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.344280][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.350953][ T1] init: Control message: Processed ctl.start for 'adbd' from pid: 588 (system_server)
[ 1285.351641][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.383464][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.390758][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.397929][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.405219][ T6289] android_work: did not send uevent (0 0 0000000000000000)
[ 1285.412470][ T6289] android_work: did not send uevent (0 0 0000000000000000)

How should I solve this problem?

My system framework is shown in the following figure:

pyh0603_0-1722960890733.png

my dts config as follow:

bq25703:

pyh0603_1-1722960906559.png

cw2015:

pyh0603_2-1722960930849.png

fusb302:

pyh0603_3-1722960941033.png

 

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,488 次查看
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Have you checked the USB voltage level?

Best regards/Saludos,
Aldo.

0 项奖励
回复

1,421 次查看
pyh0603
Contributor III

Hi Aldo,

Can you give me some tips? Thank you in advance.

@AldoG 

0 项奖励
回复

1,472 次查看
pyh0603
Contributor III

Hi, Aldo

Thank you for your reply.

When my battery voltage is greater than 8.4V, I can properly enumerate USB ADBs,the USB voltage level is 5.13V

When my battery voltage is less than 8.4V, USB adb enumeration fails, the USB voltage level is 4.3v

Looking forward to your reply @AldoG 

0 项奖励
回复