USB Video class Composite Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Video class Composite Device

1,753件の閲覧回数
Ismael_dz
Contributor II

Hello community! I got a question. For a UVC composite device with Color and sensor Camera, do I need more than 1 Video Control Descriptor? Im not sure If I simply can add the inteface and endpoint for the second camera and still use one video control of if it is needed to use two video control descriptor.

0 件の賞賛
返信
1 返信

1,735件の閲覧回数
kef2
Senior Contributor V

Hello, Ismael_dz 

Do you mean UVC class device streaming two videos simultaneously? UVC class allows many video sensors (sources) in one device but streaming just a single one at a time. Selector interface allows switching among sources. But there are no means to define two or more simultaneous video streams. That's for standard UVC device, which is recognized by built-in Windows driver.  

0 件の賞賛
返信